eCDOS Quantum V3.1 Readme

 

1. Description

This eCDOS  is synchronized with Unity Pro V7.0.

It contains binaries (Firmware / OS) and documents files needed for Modicon Quantum PLC's processors and modules upgrade.

 

Note: the most up-to-date Firmware are always available at  http://www.schneider-electric.com/

under: Automation and Control / Automation / Modicon Quantum / Download / Software/Firmware /

 

2. File organization

This eCDOS contains four folders:

- Documents

- Ethernet_modules

- Processor_modules

- RIO_modules

 

2.1. Documents

 

This folder contains the following documents:

- Quantum_compatibility_rules.pdf: describes compatibility rules and recommendations for Quantum PLC's OS

NOTICE

 

Potential Equipment Damage

We highly recommend to read this document Quantum_compatibility_rules.pdf before updating any firmware

Failure to follow these instructions can result in equipment damage.

 

 

- Quantum_65xx0_firmware_history.pdf: describes the OS enhancements for followings Quantum PLC's:

140CPU65150

140CPU65160

140CPU65260

 

- Quantum_67x6x_firmware_history.pdf : describes the OS enhancements for Quantum HSBY PLC's:

140CPU67160

140CPU67261

 

- Quantum_31110_x341x_firmware_history.pdf : describes the OS enhancements for followings Quantum PLC's

140CPU31110

140CPU43412U

140CPU53414U

 

- Quantum_Upgrade_Procedure.pdf: describes procedure  to update Quantum PLC's and Quantum Ethernet Port and modules.


 

2.2    Ethernet_modules

 

This folder contains update or upgrade files for Quantum Ethernet modules, organized in two subfolders:

- Concept_Exec_Loader

- Concept_to_Unity

- Unity

Refer to "Quantum_Upgrade_Procedure" document for upgrade process.

 

 

2.3    Processor_modules

 

This folder contains update or upgrade files for Quantum Processors modules, organized in three subfolders:

- Concept_to_Unity

- Unity_to_Concept

- Unity_Upgrade

Refer to "Quantum_Upgrade_Procedure" document for upgrade process.

 

 

2.4    RIO_modules

 

This folder contains update or upgrade files for Quantum CRP and CRA modules, organized in one subfolder:

- Unity_Upgrade

Refer to "Quantum_Upgrade_Procedure" document for upgrade process.