To UPDATE only TSXETG30XX V1.xx Procedure to update a TSXETG30xx V1.xx to TSXETG30xx V1.50 : FLASHING MODULE: Previously the Web Designer project must be already uploaded into module. 1- unzip 2- execute upgrade.bat 3- Type IP address at the prompt 4- Wait the end of transfer 5- Power cycle the module UPDATING WEB DESIGNER PROJECT: Use function ugrade target into Web Designer Software for futher detail you can refer to online help. V1.11.23MM5 Issues fixed by the patch against V1.11 official release __________________________ What is new for V1.50 : Device : - Fix issue of Modbus communication that occurs when TCP sockets stay in bad state due to the module overload. Database : - Fix issue of data recording into SQL table after loosing TCP connection between TSXETG30xx and SQL Database server. Datalogging : - Fix issue of FTP file transfer - restoring FTP connection after timeout. - Increase interoperability of datalogging files (*.csv) with new data format. Calculation : - Fix issue of truncated values of DWORD over the FLOAT maximum precision. VPN tunnel : - Fix issue of VPN blocked - TSXETG30XX detects the disconnection after 5 minutes and close the tunnel to allow a new VPN client connection. GPRS network : - Fix issue loosing network subscription and updating dyndns - TSXETG302x will restore automatically its network subscription and ip publishing PSTN and GSM data : - Fix issue in modem management,hanging up when important load of communication and low quality level of connection. NTP: - Fix issue of consumption of communication ressource when NTP server is missing.