Unity DIF V8.0

Release Notes

1.     What’s new in Unity DIF V8.0

Unity DIF V8.0 makes associated corrections and evolutions of the software Unity Dif V7.0, as described below:

o    Support for M580 and Momentum platform projects

o    New look and feel

o    Graphical representation of project differences

o   Supports XEF, ZEF, STU & STA file comparison

o    XML comparison for the selected section

o    Full Screen mode the maximize the application screen

o    Possibility to Print and Save the results

o    Comparison from Windows explorer context menu

o    Compatible with Unity Pro V8.0 , Windows 8 (32 & 64 bit) and Windows Server 2008 R2 (64 bit)

o    Quality Improvements

 

2.     Limitations

2.1.   Comparison in Offline mode only

Unity DIF will compare project files from the same PC or from remote PC. In this mode, it’s not possible to compare a project file directly with a project embedded into a PLC

2.2.   Use of Security Editor

o    If the Security is ON in Unity Pro, Unity DIF will compare project files after asking for the appropriate profile to be used. However, for Unity DIF to function correctly, the profile should have rights to at least do the following: Open an existing project, Import and Save project. In case of default Unity profile, it is recommended to use the PROGRAM profile.

o    If the Security is ON in Unity Pro, the samples cannot be used directly. Need to modify them to provide the username and password of the correct profile to be used for the comparison and recompile the samples.

o    If the Security is ON in Unity Pro with no login or avoidable login, Unity DIF will still prompt for the username and password. Provide the username and password of the correct profile to be used for the comparison

2.3.   Project Settings Limitation

Since few Project Settings have been changed from Unity Pro 5.0 onwards, the comparison of project files of earlier versions may contains added or deleted differences in the Project Settings section.

2.4.   Removal of whitespaces during Project Import / Export in Unity Pro

During project Import / Export in Unity Pro, it could happen that whitespaces at the beginning or at the end of certain language elements are being removed which leads to insignificant differences displayed in Unity DIF.

2.5.   Password Protected File

Unity Pro project file needs to be unprotected before comparing the same with Unity DIF

 

3.     Troubleshooting

3.1.   Uninstall and Reinstall of Unity Pro

In case of uninstall and reinstall of Unity Pro, the “Project Comparison” menu will disappear from the Unity Pro Tools menu. To get this menu back, reinstall or repair Unity DIF

3.2.   Comparison of STU files from a read-only server does not work

Comparison of STU files from a read-only server does not work. Copy those files into a local folder with read/write permissions to perform a successful comparison

3.3.   Chinese OS not supported

Unity DIF does not support Chinese operating system

3.4.   Unity DIF Batch mode - complete path mandatory

In batch mode while performing compare, enter the complete file path (Example: C:\Program Files\Schneider Electric\Unity Dif\Unity.stu)

3.5.   Sample Projects

All sample projects has to be built before using

 

4.     Last Minute Information

4.1.   Do not delete Unity project files during comparison

While performing comparison on Unity DIF, do not delete the files being compared. Deleting the files can lead to error conditions.

4.2.   Saving STU files with different names when program sections are opened on Unity Pro

After performing a comparison and opening a program sections on Unity Pro; performing "Save As" STU file with different names, ensure that Unity Pro instances are closed before starting next comparison or exit Unity DIF.

4.3.   Manual installation of .Net Framework 2.0 on Windows 8

Manual Installation of .Net Framework 2.0 require to run Schneider License Manager on Windows 8