Information on PCSoft software : ================================ 1- Unzip PCSoft_V1_07.zip 2- Launch " Setup.exe " 3- Start the software by launching : PCSoft.exe. 4- select your language (English, Français, Espagñol, Deutsch) For ATV212 PCSoft V1.07 is compatible with Altivar 212 software V5.1 IE51 you can use also Multi-Loader V3.11 and higher, For ATV21 PCSoft V1.06 is compatible with Altivar 21 software V1.9ie04 and with any software version compatible with it USE THE CONNEXION KIT POWERSUITE VW3 A8 106 TO CONNECT THE ALTIVAR 21 In case of availability of a new software version of PCSoft to support new functionality (addition of a new language), the user should uninstall the previous version of PCSoft before installing the new one, by " Add/Remove programs " of Windows.