Cliquer ici pour la version française


EcoStruxure Control Expert V15 Read me

 

EcoStruxure Control Expert with new Topology Manager: For a simplified automation lifecycle​

 

1.      System requirements

2.      DVD installation content

3.      Setup procedure

3.1. Steps to follow before uninstalling Control Expert

3.2. To be checked before installation.

3.3. Installing Control Expert for the first time

3.4. Installing an update of Control Expert on the computer

3.5. Custom Library

3.6. Communication drivers’ installation

4.      License right

5.      Uninstall

6.      Demo Projects

7.      Update PLC firmware

8.      Documentation & Online Help

9.      Optional libraries and Companions tools

 

1.      System requirements

 

System with Microsoft Windows 10  64bits (version 1809 minimum is mandatory , version 1903 minimum is recommended)

Note: Windows 10 32 bits is not supported

 

System:       Pentium Processor 2.4 GHz or higher, recommended 3.0 GHz

 Core i3 Processor or higher, recommended Core i7


RAM memory: 8GB minimum, recommended: 16GB

(see below note for Virtual machine)

Hard disk: minimum available free space 8 GB, recommended 20 GB

Note: EcoStruxure Control Expert V15 has been tested with Microsoft Windows 10 Enterprise 2019 LTSC (Version 1809)

 

System with Microsoft Windows Server 2019

Recommended version: Windows Server 2019, standard version

Processor recommended: 3.20GHz

RAM memory recommended: 16.0 GB

 

EcoStruxure Control Expert V15 has been tested with the following antivirus/protection active:

·         McAfee Virus Scan Entreprise V 8.8

·         Cylance Protect V2.0.1520.3 (Win7) et 2.0.1534.15 (Win10)

·         Defender for Win10

 

Control Expert requires .NET 3.5 SP1

Depending on the target Windows version and Windows configuration, .Net versions may be

      - not installed

      - installed but not enabled ( the related "windows feature"  is not set ON )

      - installed and enabled

 

Control Expert setup tries to automatically install and enable the required .Net  on the target Windows if necessary.

 

On Windows 10 and Windows Server 2019, automatic or manual installation of .Net 3.5 requires an internet connection.

And service “Windows Update” must be started in order to install the .NET Framework 3.5.

 

.NET 3.5 SP1can be downloaded from

https://dotnet.microsoft.com/download/dotnet-framework/net35-sp1

 Select: Download .NET Framework 3.5 SP1 Runtime

 

Control Expert requires .NET 4.8

.NET 4.8 is natively installed on Windows 10 version 1903 and after.

.NET 4.8 can be downloaded from

https://dotnet.microsoft.com/download/dotnet-framework/net48

Go to “Advanced downloads”, select Offline installer : Runtime

 

Virtualization:

Control Expert V15 has been successfully tested in the following configuration:

·         VMware vSphere –Hypervisor- ESXi

·         VMware Workstation 14 Pro 14.1.0

It has not been tested on Virtual Box 5.2.16-123759

Note: Ram memory of host computer must be 8GB minimum if Control Expert is used in a Virtual machine (with 4GB assigned to the Virtual machine).

DVD-ROM drive: to install the software;

DVD-ROM writer recommended

 

Display:

Min VGA (800-600).

Recommended:

·         SVGA (1024-768 or more) with high color 24 bits

·         SVGA (1280-1024 or more) for Windows 10 and Windows Server 2016

 

Pointing device:

Mouse or compatible devices. 

Access rights on the computer

Control Expert V15 needs to have Administrator access right for installing the software.

For Control Expert usage User access right are sufficient

Nevertheless, Administrator rights must be used for updating the Hardware catalog (CANopen, DTM)

PRM DTM requires administrator rights to work correctly.

 

Note: 

-       User must check that all directories used by Control Expert are accessible in read write mode.

                           Check for the Options Management: Options / General / Paths:

- Project Path

- Import / Export file path

- XVM path

- Project settings templates path

- Project settings template file

- Custom Library path

- Working drive

- Log file path

Check the directory c:\UnityProTemp (Hidden directory) has the following rights: Read, Execute and Write.

 

If these paths are not accessible an error message will appear and the requested operation will fail

-       Access rights & Multi instances: As some components are shared, when several instances of Control Expert are launched, rights access must be the same on all the instances

-       In Windows 7 , if UAC (User Account Control) is set, and if Control Expert is executed without checking "Run as Administrator", system folders can be only be accessed in read only and FFB Libset cannot be modified.

-       Start Menu: following short cuts must be executed with “Run as Administrator”:
- Remove Control Expert
- Repair Control Expert
- Types Library Update

 

 

2.      iso file installation content

 

 Directory list

 

Communication Drivers

Containing installation files for communication drivers.

 For more information, see Chapter: Communication drivers’ installation.

 

DTMLibrary, CXM Gateway DTM library, Mx80HARTGateway DTM library, NORDTMLibrary, PlaceHolder DTM Library, PME DTM Library

Containing installation files for Ethernet IP, M580 and other DTMs.
These files are automatically installed during Control Expert installation


Note 1: An update of the DTM hardware catalog is needed before first use.

 

Note 2: Some Schneider Electric communication or device DTMs are not available in Control Expert package:

Those DTMs are made available on schneider-electric.com

 

To access all Schneider-Electric DTMs :

·         Connect to http://www.schneider-electric.com

·         Support > Documents and downloads > Software/Firmware > DTM Files

 

To access Schneider-Electric DTMs managed by Control Expert :

·         Connect to http://www.schneider-electric.com

·         Support > Documents and downloads

            >> Search By current products > Control Expert

            >> Software/Firmware

 

EULA

Containing the End User License Agreement.
EULA is available in 6 languages.
It can be accessed by launching the Index.html file.

 

Extras

Containing sub folders:

·         Config DRS : Contains configuration files for Dual Ring Switches (DRS)
Following configuration can be downloaded in the switches :

 Switch 

DRS Pre configuration 

TCSESM083F23F1

C1_RIOMainRing_RIOSubRing_DIOClouds.cfg

C2_RIOMainRing_DIOSubRing_DIOClouds.cfg

C7_Master_RIOMainRing_RIOSubRing_DIOClouds.cfg

C8_Slave_RIOMainRing_RIOSubRing_DIOClouds.cfg

C9_Master_RIOMainRing_DIOSubRing_DIOClouds.cfg

C10_Slave_RIOMainRing_DIOSubRing_DIOClouds.cfg

TCSESM063F2CU1
TSCESM063F2CS1

C3_RIOMainRingFx_RIOSubRingTx_DIOCloudsTx.cfg

C4_RIOMainRingFx_DIOSubRingTx_DIOCloudsTx.cfg

C5_RIOMainRingFxTx_RIOSubRingTx_DIOCloudsTx.cfg

C6_RIOMainRingFxTx_DIOSubRingTx_DIOCloudsTx.cfg

C11_Master_RIOMainRingFxTx_RIOSubRingTx_DIOClouds.cfg

C12_Slave_RIOMainRingFxTx_RIOSubRingTx_DIOClouds.cfg

C13_Master_RIOMainRingFxTx_DIOSubRingTx_DIOClouds.cfg

C14_Slave_RIOMainRingFxTx_DIOSubRingTx_DIOClouds.cfg

C15_CRPLinkHotStandbyLD.cfg

C16_ RIOMainRingTx_RIOSubRingFx_DIOClouds.cfg

 

·         Converter Quantum M580

Contains PLCSTAT DFB for Modicon M580 (to use after migration from Quantum to M580 if PLCSTAT exists in the Quantum application).

·         Excel Import Export Tool

A tool to easily import export Control Expert variables to Excel

 

·         Operator screens

Contains M580 HSBY Operator screen template

 

Note: Files below are no more located in Extras Folder. They are now located in Control Expert installation folder (usually: C:\Program Files\Schneider Electric\Control Expert

·         DTM Audit Tool :

DtmAuditToolUI.exe

·         M580 CPU Change V1V2

M580CPUChangeV1V2.exe

This tool allows to change a M580 CPU V1.x to V2.x

 

·         M580 Application Update

M580ApplicationUpdate.exe

This tool update Control Expert Modicon M580 project containing BME NOC 03x1 from version .2 to .3 or .4

Or update a M580 project to M580 safety project

Or update a ZHW file to allow import to BMENOC within the same project

·         SD Card Writer

SdcardWriter.exe

 

The Extras folder and its subfolders are available after installation in the folder: Shared Documents \ Schneider Electric \ Control Expert

 

ISSetupPrerequisites

Containing pre required files needed for Control Expert installation.

 

NoG_Help

Containing help files for 140 NOG 111 00 module, available in German only.

 

SESU

Containing installation files for Schneider Electric Software Update tool

-       SESU tool provides automatic access to all free software updates (Hot Fix).

-       An internet connection is required to access the service.

-       Installation of the tool is taken into account by Control Expert installation.
The removing is possible from "add or remove programs" in the Windows Control Panel

  

Floating License Manager

Installation for Floating License Manager. It is not installed by Control Expert installation

 

License Manager

Installation for License Manager. It is installed by Control Expert installation

 

 

3.      Setup procedure

 

3.1. Steps to follow before uninstalling Control Expert

 

Save existing projects

For all your projects that are in a "built" status (projects that are consistent; projects that are running on a PLC):

Since Unity Pro / Control Expert V4.1 these projects are automatically saved with the extension “.auto.sta”, so archived files are available within the directory where STU files are saved.

For Unity Pro version lower than V4.1, It is mandatory to save all applications as archived files (extension .STA) using the Menu: File / Save archive…

The archive file ensures the compatibility between the different versions of Unity Pro / Control Expert. Opening this file allows keeping the application in a generated state and authorizes the connection in equal mode with the PLC (see STA compatibility rules in the section "Compatibility rules" in the ReleaseNotes.html file).

The STU files created with previous versions are not readable on this version.

Other projects in a “non built” status must be exported as source format (extension .XEF or .ZEF)

We recommend to keep all projects in the export file format (extension .ZEF)

 

3.2. To be checked before installation

 

Before the installation, please refer to the recommendations in the "Control Expert installation manual" on the electronic documentation, chapter "General points"

 

3.3. Installing Control Expert for the first time

 

The operating modes are described in "Control Expert installation manual" on the electronic documentation, chapter "Installing Control Expert for the first time"

 

3.4. Installing an update of Control Expert on the computer

 

Control Expert Licenses (Activation Id) for V14 are not vaild for V15. In other words : an Activation Id valid for V14 is also valid for V14.1

Licensing system of Control Expert V14 or V14.1 is not compatible with previous Unity Pro licensing system.

To run Control Expert V14 or V14.1 you must activate it with a Control Expert license (Activation Id). Previous Unity Pro license (Serial Number, Activation code) is no more valid.

 

3.5. Custom Libraries

 

 

After installation of Control Expert V15, the custom libraries from Unity Pro are still available in the initial installation directory C:\Documents and Settings\All Users\Application Data\Schneider Electric\Unity Pro\CustomLibset\Vx.y

This directory is not modified by Control Expert installation.

By default and whatever the version of standard library used, all applications will use the custom library located in the new directory created by Control Expert: \Documents and Settings\All Users\Application Data\Schneider Electric\Control Expert x.y\CustomLibset\Vx.y.

 

After Control Expert installation, the custom libraries from Unity Pro must be restored manually in the new default directory created by Control Expert

 

 

You can create a new custom library dedicated to previous versions of Unity Pro, by selecting the "custom library path": C:\Documents and Settings\All Users\Application Data\Schneider Electric\Unity Pro\CustomLibset\Vx.y in menu Tools/Options/General/Path.

When using Type library update tool, you have to select the right library path according to the path selected in the Options.

 

 

 

3.6. Communication drivers’ installation

 

Control Expert install Modbus, USB, XIP and Uni-Telway drivers by default.


For other drivers, please open the directory “Communication Drivers” and choose the driver through the name of the file:

 

All the following drivers are compatible with Windows 10 64bits

-         SchneiderPLCUSBDriverSuite.exe

-         SchneiderModbusDriverSuite.exe  

-         SchneiderXipDriverSuite.exe         

-         SchneiderUnitelwayDriverSuite.exe           

 

SchneiderUsbFipDriverSuite.exe and SchneiderTPCI57DriverSuite.exe are compatible with Windows 7 32/64bits and are not installed with Control Expert.

 

Ethway, FIP FPC10 / FPC20, ISAWAY and Unitelway SCP114 drivers, only compatibles with Windows XP 32bits are not delivered on Control Expert installation DVD.

They are available by download on Schneider-electric.com (Driver Pack V2.6)

 

 

4.      License right

 

If it is the first time you install the software on this computer, you need to activate a license (Activation Id) within a period of 30 days.
To register Control Expert software, you have to launch the Schneider Electric License Manager tool. Then follow the instructions displayed on the screen.

For additional information, please refer to the "Control Expert installation manual" on the electronic documentation.

Activation & Registration procedure is described in video: https://www.youtube.com/watch?v=0bSzFztSt7k (Node Locked license) or https://www.youtube.com/watch?v=jvQBbFYtOg0&t=196s (Floating License)

Registration is optional but strongly recommended (for example to allow return of licenses & transfer between computers)

Control Expert Licenses (Activation Id) for V15 are valid too for previous versions too (V14 and V14.1)

But Control Expert V14 licenses are not valid for V15.

Licensing system of Control Expert V15 or V14 is not compatible with previous Unity Pro licensing system.

To run Control Expert you must activate it with a Control Expert license (Activation Id). Previous Unity Pro license (Serial Number, Activation code) is no more valid

5.      Uninstall or Repair

 

The operating modes are described in "Control Expert installation manual" on the electronic documentation, chapter "Uninstalling Control Expert"

 

Control Expert must be uninstalled from the Windows Control Panel “Programs / Uninstall a Program” or “Add Remove Program”

       Program: Control Expert

 

Repair is only possible through installation Setup (from DVD or iso file)

Repair command does not install Libset files. To update Libset files, it is necessary to uninstall and reinstall Control Expert.

 

Important: This will not uninstall the DTM Libraries and additional Tools (SESU, License Manager) installed with Control Expert.

 

To uninstall DTM Libraries the following programs must be uninstalled:

·         EcoStruxure Control Expert PsX DTM Library

·         Schneider Electric Mx80 HART Gateway DTM Library

·         Schneider Electric BME NOR DTM Library

·         Schneider Electric PME DTM Library

·         CXM DTM

·         Schneider Electric Place Holder DTM Library

 

The following additional tool can be uninstalled, although it is highly recommended to keep them (in case other programs from Schneider Electric may use them).

·         Schneider Electric License Manager

·         Schneider Electric Software Update

 

6.      Demo Projects

 

For each type of PLC, a demo project exists and it is copied on the computer during the installation phase. All files are grouped in the user workspace, located in the folder:  ..\Users\Public\Documents\Schneider Electric\Control Expert 15.0. These files that have the Read Only attribute can be modified through the change of this attribute or user may save the project with another name.

7.      Update PLC firmware 

 

If you need to use new features of Control Expert V15 that require an update of Modicon M580/ M340/ Premium / Quantum processors or modules with the latest Firmware version, you will find the binaries and documents files needed  on the web site :
http://www.schneider-electric.com/

Under the topic: Products and Services / Automation and Control / PAC, PLC & others Controllers / <Range name> / Download / Software/Firmware / Firmware - Updates
<Range name> = Modicon M580, Modicon Premium, Modicon Quantum or Modicon M340

 

8.      Documentation and OnLine Help

 

Documentation (pdf format)

Control Expert documentation (pdf format) is only available through download (and no more with DVD in Control Expert package) in 6 languages (English, French, Chinese, Spanish, Itailan, German).

 

·         Download from Schneider-Electric.com :

 

 

https://www.se.com/en/download/document/EcoStruxureControlExpert_EN/ 

https://www.se.com/en/download/document/EcoStruxureControlExpert_FR/

https://www.se.com/en/download/document/EcoStruxureControlExpert_IT/

https://www.se.com/en/download/document/EcoStruxureControlExpert_DE/

https://www.se.com/en/download/document/EcoStruxureControlExpert_SP/

https://www.se.com/en/download/document/EcoStruxureControlExpert_ZH/  

 

Or

Site : Global

Under the topic: Support  / Download Documents & Software / Software Firmware / Software – Updates

<Product Category> = PAC, PLC & Other Controllers

<Sub-category> = PAC

<Range name> = UnityPro

< Document Type > = Technical Publications

9.  Optional libraries and Companions tools

                                                                                                                       

 

Companion

Last available version

Download link

Unity DIF

V14.0

https://www.se.com/uk/en/download/document/Unity_Dif_V140/

EFB Toolkit

V14.0

https://www.se.com/ww/en/download/document/Unity_EFB_Toolkit_V14.0/

EcoStruxure Automation Device Maintenance

V2.0

 

Unity Loader

V14

SP1

https://www.se.com/ww/en/download/document/Unity_Loader_V140_SP1/

Advantys Configuration Software

V11

http://www.schneider-electric.com/en/download/document/STBSPU1000+-+Advantys+Configuration+Software+V11.0/

 

 

Libraries and Tools

Last available version

Download link

EcoStruxure™ Control Expert - Asset Link

 

https://shop.exchange.se.com/en-US/apps/57544/ecostruxure-control-expert---asset-link

General Purpose Library for EcoStruxure™ Control Expert

(available for free)

https://shop.exchange.se.com/en-US/apps/44667/general-purpose-library-for-ecostruxure-control-expert

Enhanced LL984  V4.1 (IEC Converter)

V4.1.17 

/

TCP Open V4.0

V4.0

/

Energy Management

2018

/

Low Voltage Power Control

2018

 

Water

2018

 

AGA Gas Flow Calculations

2018

 

Model Based Control (APC)

2018

 

Fuzzy Control (APC)

2018

 

HVAC (Heat, Vent, Air Conditioning)

2018

 

PRM                   V1.3

V1.3

 

 

 

 


 

Click here for English version

 

EcoStruxure Control Expert V15 - Lisez-moi

 

 

1.      Configuration système requise. 8

2.      Contenu du DVD d’installation.. 9

3.      Procédure d'installation.. 10

3.1. Recommandations avant désinstallation. 10

3.2. A vérifier avant l’installation. 11

3.3. Première installation de Control Expert sur le poste de travail 11

3.4. Installer une mise à jour d'Control Expert sur le poste de travail 11

3.5. Bibliothèques personnalisées. 11

3.6. Installation des pilotes de communication. 12

4.      Droits de licence. 13

4.1. Enregistrement dans le cas d'une première installation. 13

4.2. Enregistrement si Control Expert V4.1 ou supérieur est déjà autorisé sur le PC. 13

4.3. Enregistrement si Control Expert V4.0 ou inférieure est déjà autorisé sur le PC. 13

4.4. Enregistrement avec Advantys Configuration Software. 14

4.5. Installation sur un nouveau poste avec une licence Control Expert V4.0 ou inférieure

5.      Désinstallation ou Réparation. 14

6.      Projets exemples. 14

7.      Mise à jour du firmware des automates. 14

8.      Documentation & Aide en Ligne. 14

9.  Librairies additionnelles et Outils Compagnons

 

 

 

1.      Configuration système requise

 

Systèmes avec Microsoft Windows 10  64bits (version 1903 minimum)

Note : Windows 10 32 bits n’est pas supporté.

 

Système : Pentium Processor 2.4 GHz ou supérieur, recommandé 3.0 GHz

 Core i3 Processor ou supérieur, recommandé Core i7


Mémoire RAM : 8 Go minimum; recommandé: 16 Go

       (voir aussi la note ci-dessous pour la virtualisation)

 

Disque dur: 8 Go d'espace disque minimum disponible, 20 Go recommandé

.

Note : EcoStruxure Control Expert V15 a été testé avec Microsoft Windows 10 Enterprise 2019 LTSC ( Version 1809)

 

Systèmes avec Microsoft Windows Server 2019

Version recommandée : Windows Server 2019, standard version.

Processeur  recommandé: 3.20GHz

Mémoire RAM recommandée: 16.0 GB

 

EcoStruxure Control Expert V15 a été testé avec ces antivirus/protection:

·         McAfee Virus Scan Entreprise V 8.8

·         Cylance Protect V2.0.1520.3 (Win7) et 2.0.1534.15 (Win10)

·         Defender for Win10

 

Remarque

Control Expert nécessite .NET 3.5

En fonction des versions de Windows et des différentes configurations, .Net peut être :

      - non installé

      - installé mais pas activé ( Le paramètre Windows correspondant est désactivé )

      - installé et activé

 

Control Expert installe automatiquement et active .Net , toutefois :

 

Sur Windows 10  et Windows Server 2016, l’installation automatique de .Net 3.5 peut nécessiter une connexion internet,

Et le service “Windows Update” doit être démarré pour pouvoir installer .NET Framework 3.5.

 

Si l’installation automatique de .Net 3.5  échoue, consulter la note technique Microsoft :

 

      - Installation de .NET Framework 3.5 :

https://dotnet.microsoft.com/download/dotnet-framework/net35-sp1

 Select: Download .NET Framework 3.5 SP1 Runtime

 

Control Expert nécessite .NET 3.5

Installation de .NET:

https://dotnet.microsoft.com/download/dotnet-framework/net48

de “Advanced downloads”, selectionner Offline installer : Runtime

 

           
Virtualisation:

Control Expert V15 a été testé avec succès dans les configurations suivantes : 

 Mémoire RAM : 8 Go minimum pour l’ordinateur hôte (avec 4 Go minimum affectés à la machine virtuelle)

 

Lecteur DVD-ROM : pour l’installation du logiciel

Recommandé : un graveur de DVD-ROM

Affichage :

Min VGA (800-600).

Recommandé :

·         SVGA (1024-768 ou plus) avec couleurs vraies sur 24 bits.

·         SVGA (1280-1024 ou plus) sur Windows 8.1 et Windows Server 2016

 

 

Système de pointage :

Une souris ou périphérique compatible.

Accès Web :

L’enregistrement par le Web nécessite un accès Internet.

Droits d'accès du poste de travail

Control Expert V15 nécessite d'avoir les droits d'accès administrateur pour installer le logiciel.
Pour l’utilisation d’Control Expert, les droits d’accès utilisateurs sont suffisants.

Néanmoins des droits d'administrateur doivent être utilisés pour mettre à jour le catalogue du matériel (CANopen, DTM)

La DTM PRM nécessite des droits administrateur pour fonctionner correctement.

Note: 

-       L'utilisateur doit vérifier que tous les répertoires utilisés par Control Expert sont accessibles en lecture écriture

Vérifier les Paramètres des options: Options / Général / Chemins

- Chemin du projet
- Chemin du fichier d’import / export
- Chemin du XVM
- Chemin des modèles de paramètres de projet
- Fichier du modèle de paramètres de projet
- Chemin de bibliothèque personnalisée
- Lecteur de travail
- Chemin des fichiers d’historique

Vérifier que le répertoire C:\UnityProTemp (répertoire caché par défaut) dispose aussi des droits en lecture, exécution et écriture

 

Si ces chemins ne sont pas accessibles un message d’erreur apparaitra et les opérations demandées échoueront.

 

-       Comme certains composants sont partagés, lorsque plusieurs instances de Control Expert sont lancées, les droits d'accès doivent être les mêmes sur toutes les instances

 

Menu Démarrer : Les commandes suivantes doivent être exécutées par “Exécuter en tant qu’administrateur” :

 

-  Remove Control Expert (Désinstaller Control Expert)
-  Repair Control Expert (Réparer Control Expert)
-  Types Library Update (Mise à jour Libraries)

-        

 

2.      Contenu du DVD d’installation

 

 Liste des répertoires

 

Communication Drivers

Contenant les fichiers d’installation des drivers de communication.

Pour plus d’information, voir le chapitre : Installation des pilotes de communication.

 

DTMLibrary

Contenant les fichiers d’installation des DTM utilisées par les modules Ethernet IP.
Ces fichiers sont installés automatiquement à l’installation d’Control Expert.
Note 1 : Une mise à jour du catalogue DTM, est nécessaire lors de la première utilisation.

 

Note 2 : Certaines DTMs de communication ou d’équipement  Schneider Electric ne sont pas disponibles dans le DVD Control Expert V14

Ces DTMs sont disponibles sur le site schneider-electric.com

 

Accés à l’ensemble des DTMs Schneider-Electric :

·         Connecter http://www.schneider-electric.com

·         Support > Documents and downloads > Software/Firmware > DTM Files

 

Accés aux DTMs Schneider-Electric DTMs utilisables avec Control Expert :

·         Connecter http://www.schneider-electric.com

·         Support > Documents and downloads

            >> Search By current products > Control Expert

            >> Software/Firmware

 

 

EULA

Contenant le contrat de licence utilisateur final.
Le contrat est disponible en 6 langues. Il peut être consulté en lançant le fichier Index.html.

 

Extras

Contenant les sous répertoire

·         Config DRS :
Contenant les fichiers de configuration pour les  Switchs Dual Ring (DRS)
Les configurations suivantes peuvent être chargées dans les Switchs :

 Switch 

DRS Pre configuration  

TCSESM083F23F1

C1_RIOMainRing_RIOSubRing_DIOClouds.cfg

C2_RIOMainRing_DIOSubRing_DIOClouds.cfg

C7_Master_RIOMainRing_RIOSubRing_DIOClouds.cfg

C8_Slave_RIOMainRing_RIOSubRing_DIOClouds.cfg

C9_Master_RIOMainRing_DIOSubRing_DIOClouds.cfg

C10_Slave_RIOMainRing_DIOSubRing_DIOClouds.cfg

TCSESM063F2CU1
TSCESM063F2CS1

C3_RIOMainRingFx_RIOSubRingTx_DIOCloudsTx.cfg

C4_RIOMainRingFx_DIOSubRingTx_DIOCloudsTx.cfg

C5_RIOMainRingFxTx_RIOSubRingTx_DIOCloudsTx.cfg

C6_RIOMainRingFxTx_DIOSubRingTx_DIOCloudsTx.cfg

C11_Master_RIOMainRingFxTx_RIOSubRingTx_DIOClouds.cfg

C12_Slave_RIOMainRingFxTx_RIOSubRingTx_DIOClouds.cfg

C13_Master_RIOMainRingFxTx_DIOSubRingTx_DIOClouds.cfg

C14_Slave_RIOMainRingFxTx_DIOSubRingTx_DIOClouds.cfg

C15_CRPLinkHotStandbyLD.cfg

C16_ RIOMainRingTx_RIOSubRingFx_DIOClouds.cfg

 

·         Excel Import Export Tool

Contient un outil permettant l’import/export des variables Control Expert vers Excel.

 

·         Operator screens

Contient un modèle d’écran de Dialogue Opérateur pour  M580 HSBY.

 

·         Converter Quantum M580

Contient le DFB PLCSTAT pour Modicon M580 (à utiliser après migration de Quantum vers M580 si PLCSTAT était utilisé dans l’application Quantum).

 

 

Note : les utilitaires ci-dessous ne sont plus localisés dans Extras , mais dans le dossier d’installation de Control Expert (par exemple: C:\Program Files\Schneider Electric\Control Expert

·         DTM Audit Tool :

DtmAuditToolUI.exe

·         M580 CPU Change V1V2

M580CPUChangeV1V2.exe

Pour mettre à jour un CPU M580 V1.x en V2.x

 

·         M580 Application Update

M580ApplicationUpdate.exe

Pour mettre à jour un projet Control Expert Modicon M580 avec BME NOC 03x1 version .2 en .3. ou .4

Ou mettre à jour un projet M580 vers un projet M580 Safety

Ou mettre à jour un fichier d’export ZHW pour permettre l’import dans un module BMENOC dans un même

·         SD Card Writer

SdcardWriter.exe

 

Le dossier Extras et ses sous répertoires sont disponibles après installation dans le répertoire Documents partagés\Schneider Electric\Control Expert

 

ISSetupPrerequisites

Contenant les fichiers pré requis, nécessaires à l’installation d’Control Expert

 

NoG_Help

Contenant les fichiers d’aide du module 140 NOG 111 00 disponible en allemand uniquement.

 

SESU

Contenant les fichiers d’installation du logiciel Schneider Electric Software Update.

-   L’outil SESU fournit un accès automatique aux mises à jour gratuites du logiciel (Hot Fix)

-   Une connexion Internet est nécessaire pour accéder au service.

-   L’installation de cet outil est prise en compte par l’installation d’Control Expert.
La désinstallation est possible à partir de “ajouter ou supprimer des programmes“ dans le panneau de configuration Windows.

 

 

 

 

3.      Procédure d'installation

 

3.1. Recommandations avant désinstallation

 

Sauvegarde des projets existants

Pour tous les projets qui sont dans un statut "généré" (projets cohérents; projets en cours d'exécution sur des automates):

Depuis la version V4.1 de Unity Pro / Control Expert, ces projets sont automatiquement enregistrés avec l'extension ".auto.sta", les fichiers ainsi archivés sont disponibles dans le répertoire où les fichiers STU sont sauvegardés.

Pour les versions de Unity pro inférieure à V4.1, Il est indispensable d'enregistrer toutes les applications sous la forme de fichiers d'archive (extension .STA) en utilisant le Menu : Fichier / Archiver…

Le fichier d’archive assure la compatibilité des applications entre les différentes versions de Control Expert / Unity Pro. L’ouverture de ce fichier permet de conserver l’application dans un état généré et autorise la connexion en mode "égal" avec l’automate. (voir règles de compatibilité STA dans la section "Règles de compatibilités » dans le fichier ReleaseNotes.html)

Les fichiers STU créés à l'aide de versions précédentes ne peuvent pas être lus sur cette version.

Tous les projets dans un état "non généré" doivent être exportés en format source (extension .XEF ou ZEF)

Il est aussi recommandé de conserver tous les projets sous un format exporté (extension ZEF).

 

3.2. A vérifier avant l’installation

 

Avant d'installer le logiciel, veuillez-vous reporter aux recommandations du "Manuel d'installation de Control Expert" dans la documentation électronique, dans le chapitre "Points généraux"

 

3.3. Première installation de Control Expert sur le poste de travail

 

Les modes opératoires sont décrits dans le "Manuel d'installation de Control Expert" dans la documentation électronique, dans le chapitre "Installer Control Expert pour la première fois"

 

3.4. Installer une mise à jour de Control Expert sur le poste de travail

 

Control Expert Licenses (Activation Id) for V14 are not vaild for V15. In other words : an Activation Id valid for V14 is also valid for V14.1

Pour utiliser Control Expert vos devez activer votre License Control Expert (Activation Id) à l’aide de l’outil Schneider Electric License Manager.

Les anciennes licences Unity Pro (Numéro de Série, Code d’enregistrement) ne sont plus utilisables avec Control Expert

Les licences (Activation Id) de Control Expert V14 ne sont pas compatibles avec V15. Une licence V15 valide est nécessaire pour utiliser Control Expert V15.

Les licences (Activation Id) de Control Expert V15 sont compatibles avec V14 et V14.1.

 

3.5. Bibliothèques personnalisées

 

 

Après l'installation de Control Expert V14.1, les bibliothèques personnalisées de Unity Pro sont toujours disponibles dans le répertoire d’installation initial : C:\Documents and Settings\All Users\Application Data\Schneider Electric\Unity Pro\CustomLibset\Vx.y

Ce répertoire n’est pas modifié par l’installation de la nouvelle version Control Expert. Par défaut toutes les applications utiliseront les bibliothèques personnalisées situées dans le nouveau répertoire créé par Control Expert : C:\Documents and Settings\All Users\Application Data\Schneider Electric\Control Expert x.y\CustomLibset\Vx.y.

 

Après l'installation de Control Expert, les bibliothèques personnalisées de Unity Pro devront être restaurées manuellement dans le dans le nouveau répertoire créé (par défaut).par Control Expert.


Vous pouvez créer des bibliothèques personnalisées dédiées à Unity Pro, en sélectionnant le "chemin des bibliothèques personnalisées": C: \ Documents and Settings \ All Users \ Application Data \ Schneider Electric \ Unity Pro \ CustomLibset \ V13.1 dans le menu Tools / Options / General / Path.
Lors de l'utilisation de l'outil de mise à jour des bibliothèques de type, vous devez sélectionner le chemin des bibliothèques personnalisées correspondant à celui sélectionné dans les options.

 

 

 

 

3.6. Installation des pilotes de communication

 

Control Expert vous propose d’installer par défaut les pilotes Modbus, USB , XIP et Uni-Telway.


Pour les autres pilotes, veuillez ouvrir le répertoire “Communication Drivers” et choisir le pilote en fonction de son nom de fichier :

 

Les drivers suivant sont compatible avec Windows 10 64bits

 

-         SchneiderPLCUSBDriverSuite.exe

-         SchneiderModbusDriverSuite.exe

-         SchneiderXipDriverSuite.exe

-         SchneiderUnitelwayDriverSuite.exe

 

Les drivers suivant sont compatible avec Windows Seven 32/64bits, et ne sont pas installés avec Control Expert.

-         SchneiderUsbFipDriverSuite.exe

-         SchneiderTPCI57DriverSuite.exe

 


Les drivers Ethway, FIP FPC10 / FPC20, ISAWAY et Unitelway SCP114 drivers sont uniquement compatible avec Windows XP 32bits et ne sont pas livrés sur l’installation d’Control Expert.
Ils sont disponibles par téléchargement sur le site Schneider-electric.com (Driver Pack V2.6)

 

4.      Droits de licence

 

Vous devez activer votre licence (Activation Id) dans un délai de 30 jours.

Pour enregistrer le logiciel Control Expert, vous devez lancer l'outil d'enregistrement Schneider Electric License Manager

Les procedures d’Activation & Registration sont décrites: https://www.youtube.com/watch?v=0bSzFztSt7k (Node Locked licence) ou https://www.youtube.com/watch?v=jvQBbFYtOg0&t=196s (Floating Licence)

Les licences de Control Expert V14 ne sont pas valides sur la version V15.

 

5.      Désinstallation ou Réparation

 

Les modes opératoires sont décrits dans le "Manuel d'installation de Control Expert" dans la documentation électronique, dans le chapitre "Désinstaller Control Expert".

 

Control Expert doit être désinstallé depuis le panneau de configuration Windows “Programmes / Désinstaller un Programme”

       Programme : Control Expert

 

La commande "Réparer Control Expert"  n’est disponible que depuis le fichier d’installation (DVD ou fichier iso).

La commande "Réparer Control Expert" ne répare pas les fichiers de Librairies. Pour cela il est nécessaire de désinstaller et réinstaller Control Expert.

 

Remarque Importante : La désinstallation de Control Expert ne désinstalle pas automatiquement les librairies DTM ni les outils (SESU, License Manager) installés avec Control Expert.

Pour désinstaller les librairies DTM, les programmes suivants doivent être désinstallés :

·         EcoStruxure Control Expert PsX DTM Library

·         Schneider Electric Mx80 HART Gateway DTM Library

·         Schneider Electric BME NOR DTM Library

·         Schneider Electric PME DTM Library

·         CXM DTM

·         Schneider Electric Place Holder DTM

 

Les outils suivants (installés par Control Expert) peuvent être désinstallés, mais il est recommandé de les conserver car ils peuvent être utilise par d’autres logiciels de Schneider Electric.

·         Schneider Electric License Manager

·         Schneider Electric Software Update

 

 

6.      Projets exemples

 

Pour chaque type d'automate, il existe un projet exemple qui est copié sur le poste de travail lors de l'installation du logiciel. Les fichiers sont regroupés dans l'espace de travail des utilisateurs, dans le répertoire : :  …\Public\Documents\Schneider Electric\Control Expert 14.1 Ces fichiers en lecture seule, peuvent être modifiés en changeant la propriété du fichier ou en sauvegardant le projet sous un autre nom.

7.      Mise à jour du firmware des automates

 

Désormais, firmwares des automates sont disponibles sous forme électronique par téléchargement.

Si vous devez utiliser les nouvelles fonctionnalités de Control Expert V14.1 qui demandent une mise à jour des processeurs ou des modules M580/Premium/Quantum/M340 avec la dernière version du Firmware, vous trouverez les fichiers binaires et les documents requis sur le site : 
http://www.schneider-electric.com/

Sous la rubrique :   Produits et Services / Automatisme et Contrôle / Automatisation /  <Gamme> / Téléchargement / Logiciel / Micrologiciels - mises à jour

<Gamme> = Modicon M580, Modicon Premium, Modicon Quantum ou Modicon M340

 

 

 8.      Documentation et Aide en Ligne 

 

Documentation (format pdf)

La documentation Control Expert (pdf format) n’est disponible que par téléchargement  (et pas sur le  DVD Control Expert) depuis Schneider-Electric.com en 6 langues (Anglais, Français, Chinois, Espagnol, Italien, Allemand).

 

https://www.se.com/en/download/document/EcoStruxureControlExpert_FR/

 

 

Ou bien

Site : Global

Support  / Download Documents & Software / Software Firmware / Software – Updates

<Product Category> = PAC, PLC & Other Controllers

<Sub-category> = PAC

<Range name> = UnityPro

< Document Type > = Technical Publications

 

9.        Librairies additionnelles et Outils Compagnons

See : 9.  Optional libraries and Companions tools