© Schneider Electric, 1995-2012; All Rights Reserved

 

Accéder à la version française

 

OPC Factory Server V3.40 - Read Me

        Table of content

 

  1. What’s new in OPC Factory Server V3 40

  2. Last Minute Information

  3. DVD Content

1      What’s new in OPC Factory Server V3.40

Time Stamping

 

    OFS V3.40 is able to manage at source time stamped digital data natively, transparently and with guarranty not to loose any data in case of burst of events .OFS V3.40 gets the time stamped data directly from the sources, which can be either BMX ERT module (1ms resolution) or any regular x80 digital remote IO (10ms resolution) behind x80 performance IO adapter.  

 

 

 

OPC UA Compatibility

 

 

    OFS V3.40 brings also connectivity to OPC UA (Unified Architecture) clients via an OPC UA 'wrapper', wrapper intending to convert OPC DA protocol into OPC UA protocol . Note that is OFS is getting at source time-stamped data , then the data delivered to the OPC UA wrapper will be also at source time stamped.

 

2      Last minute information  

Be aware that there is now a new folder in OFS DVD, named 'Extras'

This folder conatins :

            - A utility named OFSTimeStampHelper, intended to help user to define setting parameters of OFS when used in a configuration with at source time stamped data

            - A System Time Stamping User Guide

            - HotFix and patches for Unity Pro V7 and Products required to manage at source time stamped data

 

 

       Note1 : Switch to "System Mode"

 

               After install of UnityPro_V70_HF1, user has to switch in “system mode” to use this new mode :

                  Menu : Tools / Project Settings / Time

                      Time Stamping Mode = System

 

 

       Note 2 : SOE uncertain variable set in applicative mode

 

               If the application containing ERT modules in local rack was created in “applicative mode” and if this application uses variables “SOE uncertain” an error will occur when     

               building the application.

               User will have to change the edge of each SOE variable from “both” to “none” and then again to “both” to remove error.

 

 

       Note 3 : Uncertain sequence of events

 

              In some very particular conditions, it may happen that an uncertain sequence of events on the same event source (BMX-CRA) begins with the log of two consecutive

              SOE-UNCERTAIN events (0->1)  and ends with only one SOE-UNCERTAIN event (1->0 ) . In this case please consider that the uncertain sequence of events begins at

              the time specified in the first SOE-UNCERTAIN event (0->1).

 

       Note 4 : Signed .Net applications or Assemblies can take longer time to launch

 

       This delay is due to the verification of the Microsoft Certificate Revocation List before loading the application

 

 

Note 5 : unlike it is mentionned in the OFS user manual, #TSEventSyncro operation can be performed before or after the event group activation.

 

 

 

 

 

3      DVD Content

Communication Drivers

Containing installation files for communication drivers.

For more information, see Chapter: Communication drivers installation.

    OPC Factory Server install Modbus, USB and Uni-Telway drivers by default.


   
All the following drivers are compatible with Windows XP 32bits, Vista 32/64bits and Seven 32/64bits.

-         SchneiderPLCUSBDriverSuite.exe

-         SchneiderModbusDriverSuite.exe  

-         SchneiderXipDriverSuite.exe         

-         SchneiderUsbFipDriverSuite.exe   

-         SchneiderUnitelwayDriverSuite.exe           

-         SchneiderTPCI57DriverSuite.exe   

 

Then follow instructions appearing in the dialogs.

 

Ethway, FIP FPC10 / FPC20, ISAWAY and Unitelway SCP114 drivers, only compatibles with Windows XP 32bits are not delivered on OPC Factory Server DVD.

They are available by download on www.schneider-electric.com  

  

EULA

Containing the End User License Agreement.
EULA is available in 6 languages.
It can be accessed by launching the Index.html file.

 

 

Extras

Containing 3 sub folders.

-    OFS TimeStamp Helper : OFS TimeStamp Helper is intended to help you to define setting parameters of OFS when used in a configuration with "at source times tamping" service depending of your needs in term of events detection capability.

System TimeStamping User Guide : Contains a specific user guide for System Time Stamping functionalities

TimeStamping HotFix : Contains 3 HotFix for respectively UnityPro V70 ,BMX ERT  and BMX CRA.

   

 

Access the English version

OPC Factory Server V3.40 - Lisez-moi

Table des matières

  1. Nouveautés OPC Factory Server V3.40

  2. Last minute information

  3. Contenu du DVD

 

1      Nouveautés OPC factory Server V3.40

Horodatage à la source 

 

OFSV3.40 gère des données horodatée à la source  de manière transparente, sans nécessiter de programme applicatifs tout en garantissant de ne pas perdre d'évènements même en cas d'avalanches. OFS V3.40 fait l'acquisition de ces évènements directement à la source, qui peuvent être soit un module d'ES de type BMX ERT (1ms résolution) ou tout ES x80 TOR standard derrière un adaptateur x80 'performance'  (10 ms résolution).

 

 

Compatibilité OPC UA

 

 

OFS V3.40 apporte egalement la compatibilité avec le protocole OPC UA (Unified Architecture) grace à un wrapper, convertissant  le protocole OPC DA fournit par OFS en protocole OPC UA standard.

 

2      Last Minute Information

Un nouveau répertoire 'Extras'  sur le DVD OFS V3.40 contient

-          Un utilitaire appelé OFSTime StampHelper, destiné à aider l'utilisateur à définir les paramètres optimum requis dans les configurations gérant des données horodatées à la source

-          Un guide de l'utilisateur des données horodatées à la source

-          Un hot fix pour Unity Pro V7

-          Des patches pour les firmwares des différents produits requis dans les configurations gérant des données horodatées à  la source

 

 

 

Remarque 1 : Sélection du mode “Systeme”

 

             Après installation de UnityPro_V70_HF1, l’utilisateur doit sélectionner le mode Système dans les Options du Projet pour bénéficier de cette la fonctionnalité.

               Menu : Outils / Options du Projet / Heure

                   Mode Horodatage = Système Variable

 

 

Remarque 2 : SOE incertain définie en mode applicatif

 

      Dans une application utilisant un module ERT en rack local, dont le mode Horodatage est “Applicatif” , et dans laquelle les variables SOE incertain sont utilisées, si le mode horodatage est changé en « Système », alors une erreur sera détectée à la génération de l’application L’utilisateur devra modifier le front des variables (colonne Horodatage de l’éditeur de variable) de « deux fronts » à « aucun », puis de nouveau à « deux fronts » pour supprimer l’erreur.

 

 

Remarque 3 :  Sequence d'évènements incertains

 

      Dans certains cas particuliers, il peut arriver qu'une séquence d'évènements incertains issue de la meme source d'évènements (BMX-CRA) commence avec l'enregistrement de deux évènements consécutifs SOE-UNCERTAIN (0 -> 1) et se termine avec l'enregistrement d'un seul évènement SOE-UNCERTAIN (1 -> 0). Dans ce cas il faut considérer que la séquence d'évènements incertains commence au temps indiqué par le premier évènement SOE-UNCERTAIN (0->1).

 

 

  Remarque 4 : Les applications .Net signées peuvent prendre plus de temps pour se lancer

 

       Ce retard est dû à la vérification de la Microsoft Certificate Revocation List avant le chargement de l'application

 

 

  Remarque 5 : contrairement à ce qui est mentionné dans le manuel utilisateur,  #TSEventSyncro peut être exécuté avant ou aprés l’activation du groupe d’événements.

 

3      Contenu du DVD

 Communication Drivers

Contenant les fichiers d’installation des drivers de communication.

    OPC factory Server vous propose d’installer par défaut les pilotes Modbus, USB et Uni-Telway.

   

    Pour les autres pilotes, veuillez ouvrir le répertoire “Communication Drivers” et choisir le pilote en fonction de son nom de fichier :

    Tous les drivers suivant sont compatible avec Windows XP 32bits, Vista 32/64bits et Seven 32/64bits.

            -         SchneiderPLCUSBDriverSuite.exe

            -         SchneiderModbusDriverSuite.exe

            -         SchneiderXipDriverSuite.exe

            -         SchneiderUsbFipDriverSuite.exe

            -         SchneiderUnitelwayDriverSuite.exe

            -         SchneiderTPCI57DriverSuite.exe

Puis suivez les instructions apparaissant dans les boîtes de dialogue.

Les drivers Ethway, FIP FPC10 / FPC20, ISAWAY et Unitelway SCP114 drivers sont uniquement compatible avec Windows XP 32bits et ne sont pas livrés sur l’installation d’OPC Factory Server DVD.
Ils sont disponibles par téléchargement sur le site www.schneider-electric.com

 

 

 

 

EULA

Contenant le contrat de licence utilisateur final.
Le contrat est disponible en 6 langues. Il peut être consulté en lançant le fichier Index.html.

 

 

 

Extras

Contenant 3 sous repertoires :

-    OFS TimeStamp Helper L'outil est destiné à vous aider à définir les paramètres de réglage d'OFS lorsqu'il est utilisé dans une configuration d' "Horodatage à la source" en fonction de vos besoins en terme de capacité de détection des événements.

System TimeStamping User Guide : Contient un guide utilisateur spécifique relatif au fonctionnalités d' Horodatage Systeme.

TimeStamping HotFix : Contient 3 HotFix pour respectivement UnityPro V70 ,BMX ERT  et BMX CRA.