Procedure to update a TSXETG1000 to V1.1 IE14 : ----------------------------------------------- 1- unzip the file UpgradeFw.zip 2- In a DOS command prompt, launch upgrade @IP ETG1000 (ex: upgrade 192.168.2.10) 3- Wait the end of transfer 4- Power cycle the ETG1000 V1.1 IE14 Features provided by the version IE14 against official release -------------------------------------------------------------- 1. Fix the issue of continuous 'Brodcast ARP' during 15 minutes after 497 days of running ******************************************************************************************************* * Important Note: * * * * Use a reliable Ethernet link for the update module : * * a link error during transfer could lead to a no working module * * (preferred: direct link, not recommanded: a remote link) * * * * * * *******************************************************************************************************