Advanced UPS Setups
Add UPS Setup
In an Advanced UPS configuration,
a single instance of PowerChute Network Shutdown can monitor multiple
UPS setups and initiate graceful shutdown of equipment based on different
redundancy levels. Each setup can be a single UPS or a UPS group. A single
UPS setup is represented by the
icon. A UPS group
is represented by the
icon.
For example, one setup may be a group of UPS's that are configured with N+2 redundancy. Another setup may be a single UPS.
On the UPS Details page of the Setup Wizard, click the + Add UPS(s) button to create a new setup.
To create a setup with a single UPS, on the Configure UPS Setup dialog choose Single UPS:
Enter a UPS Setup Name (with a maximum of 20 ASCII characters)
Click the + Add IP Address button and enter the IP address of the Network Management card in the UPS. Click OK.
Click OK to complete Single UPS Setup.
To create a setup with a group of UPS devices, choose UPS
Group:
Enter a UPS Setup Name (with a maximum of 20 ASCII characters)
Click the + Add IP Address button and enter the IP address of the Network Management card in the UPS. Click OK.
Repeat for each of the UPS devices to be added to the UPS group. A minimum of 2 IP addresses is required to set up a UPS Group.
Click OK to complete Group UPS Setup.
Repeat for each UPS setup required.
To edit a UPS Setup, click the
icon. To delete a UPS
setup, click the
icon.
Click the Next button to go to the next step
of the Setup Wizard.
|
PowerChute has been tested with a total of 16 NMCs in an advanced configuration. However it is possible to configure for more than 16 NMCs in this configuration. |
For detailed information, please view the “Using PowerChute Network Shutdown in an Advanced Redundant Setup” Application Note here.