Start-up and Shut-down Scheduling

 

PowerChute does not directly support the start-up and shut-down scheduling feature as it is available from the Network Management Card. For more information on supported scheduling features, refer to the NMC User Guide.