SSH Settings
PowerChute Network Shutdown can be configured to execute commands on a remote host via an SSH connection. To create an SSH action, click Add Action and configure the following:
- Name: A unique name for each SSH action of a length less than or equal to 255 ASCII characters.
- Configure one of the following authentication methods:
- User Name and Password: Enter the user name and password to connect to the remote host.
- User Name, SSH Key File Path and SSH Key File Password: Specify the path to a shared SSH key. This option requires you to generate an SSH key and copy it to your target systems. See SSH Command File Location.
- IP Addresses/FQDN and Port: The IP address or Fully Qualified Domain Name (FQDN) and port of the target SSH component.
- Path to SSH command file: You must specify the full path name of the command file, including the disk drive or volume number. See SSH Command File Location.
- SSH Action Delay: Enter the amount of time, in seconds, that PowerChute will wait before connecting to the remote host and begin sending commands. The default value is 0.
- SSH Action Duration: Enter the amount of time, in seconds, for the SSH action to complete before proceeding with the rest of the shutdown sequence.

Using the SSH Action Duration field, you must allow sufficient time for all your SSH actions to complete.
- Execute SSH Action:
- On Startup: Execute the SSH command file when the PowerChute service re-starts. In an advanced configuration, the SSH command file is executed when the critical UPS event is resolved.
- Before VM Shutdown: Execute the SSH command file before the User VM Migration and Shutdown step.
- Before Host Shutdown: Execute the SSH command file before host shutdown.
-
After Host Shutdown: Execute the SSH command file after host shutdown.
- Enable SSH Action: Allows you to enable or disable the configured SSH action. This checkbox is enabled by default when a new SSH action is created.
|
|
NOTES:
|
SSH Command File Location
The SSH key file, if configured, and command file must be located in the user_files folder, or a sub-folder, in the PowerChute installation directory. If the default installation directory was chosen during installation, this location will be:
-
C:\Program Files\APC\PowerChute\user_files for Windows systems
-
/opt/APC/PowerChute/user_files/ for Linux systems
|
|
NOTE: If you are upgrading to PowerChute v5.2, any key files and/or command files used in a previous version of PowerChute must be manually added to the user_files folder. If the files are not added to the directory, you will see the below errors in the Event Log: ERROR: The ini contains an invalid value for ssh_command_file_path in section SSHAction0. ERROR: The ini contains an invalid value for ssh_keyfile_path in section SSHAction0. It is strongly recommended you validate your configuration after an upgrade. |
SSH Settings in an Advanced UPS Configuration
In an Advanced UPS configuration, SSH actions can be enabled and disabled for each UPS setup.
The
symbol indicates that an SSH action is enabled in the main SSH Settings screen. To run an SSH action for a particular UPS setup, enable the checkbox next to the
symbol.
SSH actions that are not enabled do not display the
symbol. These disabled actions will not be executed if enabled for a UPS setup.