SNMPv3 Configuration
Select Enable SNMPv3 access to configure the SNMPv3 settings. Select Add Profile and configure:
- User Name: In SNMPv3, all GET and SET requests and SNMP Traps are matched to a user profile by the User Name. Enter a user name of a length less than or equal to 32 ASCII characters.
- Authentication Protocol: Select MD5, SHA-1 or SHA-2 (SHA256 or SHA512) protocol. It is recommended to use an SHA-2 protocol, if the NMS supports it.
- Authentication Passphrase: Enter an authentication password for the protocol selected, of 8-32 ASCII characters.
- Privacy Protocol: Select AES-128, AES-192*, AES-192 Ex†, AES-256* , AES-256 Ex†, or DES. It is recommended to use the AES-256 protocol, if the NMS and PowerChute JRE support it.
- Privacy Passphrase: Enter a privacy password for the encryption protocol selected, of 8-32 ASCII characters.
- Access Type:
- Disable: No SNMP GET or SET requests are permitted.
- Read: Only SNMP GET requests are permitted.
- Read/Write: SNMP GET and SET requests are permitted.
|
It is not recommended to use the MD5 protocol. |
To edit an existing SNMPv3 user profile, click the
button. To delete an SNMPv3
user profile, click the
button.
Click Apply to save the SNMPv3 configuration.
|
Certain Network Management Systems require the SNMP Engine ID to communicate via SNMP. The SNMP Engine ID is displayed on the SNMP Settings page of the PowerChute user interface. |