SSH Action Events
|
|
Click an event below for more information. |
- Running SSH Action: [Action].Running SSH Action: [Action].
PowerChute is running the SSH action [Action] on the remote host.
- SSH Action [Action] has already run.SSH Action [Action] has already run.
In an advanced UPS configuration, PowerChute runs each SSH action once for each host in the advanced group. This may result in multiple hosts attempting to run the same SSH action at the same time.
This event is shown if a SSH action has already run on a host in the advanced group.
- SSH Action [Action] has completed.SSH Action [Action] has completed.
PowerChute has successfully completed executing the SSH action [Action] on the remote host.
- SSH Action [Action] has not completed within the configured duration.SSH Action [Action] has not completed within the configured duration.
The SSH action [Action] could not complete as insufficient time was configured. Ensure sufficient time is provided in the SSH Action Duration field in the SSH Settings screen for your SSH actions to complete.