Java Update Events
|
|
Click an event below for more information. |
- Updating Java using [Java file].Updating Java using [Java file].
PowerChute is attempting to update the Java version used by PowerChute to [Java file]. Allow 2-3 minutes for the Java update to complete.
- Java has successfully updated. Restarting PowerChute.Java has successfully updated. Restarting PowerChute.
The Java version used with PowerChute has successfully updated. The PowerChute service will restart for changes to take effect.
- Unable to update Java. See error.log for details.Unable to update Java. See error.log for details.
PowerChute was unable to update the Java version used with PowerChute. For more information, see error.log.