Configurable Environmental Events
The following events are logged and event actions are carried out even if they occur on a single UPS in a Redundant or Parallel UPS configuration.
|
|
Click an event below for more information. |
- Ambient
Temperature Out Of Range Probe X. Ambient
Temperature Out Of Range Probe X.
The temperature exceeds the threshold configured for the Environmental temperature probe.
- Ambient
Temperature In Range Probe X. Ambient
Temperature In Range Probe X.
The temperature no longer exceeds the threshold configured for the Environmental temperature probe.
- Humidity
out of Range Probe X. Humidity
out of Range Probe X.
The humidity exceeds the threshold configured for the Environmental humidity probe.
- Humidity
In Range Probe X. Humidity
In Range Probe X.
The humidity no longer exceeds the threshold configured for the Environmental humidity probe.
- Communication
lost with Environmental Monitor. Communication
lost with Environmental Monitor.
PowerChute has stopped receiving data from the Environmental Monitoring Card or the probe has been removed from the Universal I/O (UIO) port on the NMC.
Check to see that the Environmental Monitoring Card is firmly inserted in its slot and has power. Check that environmental monitoring information is accessible through the NMC user interface.
If PowerChute cannot communicate with the NMC you will need to correct that problem first.
- Communication
established with the Environmental Monitor. Communication
established with the Environmental Monitor.
PowerChute Network Shutdown is receiving data from the Environmental Monitoring Card/Probe.
- Contact
X Alarm.Contact
X Alarm.
One of the environmental input contacts is in an alarm state. Check in the location being monitored by this contact.
- Contact
X Normal.Contact
X Normal.
One of the environmental input contacts has returned to a normal condition.