Event Configuration
When UPS events occur, PowerChute can be configured to log the event, notify users, execute a command file or initiate a system shutdown through the Configure Events screen.
The
symbol
indicates that the action is enabled for this event while the
symbol indicates that the
action is not enabled.
|
Descriptions of events are in the PowerChute Events and Logging sections. |