HPE SimpliVity Support for VMware

 

If you have an HPE SimpliVity Cluster with ESXi as your hypervisor, you can enable HPE SimpliVity support for PowerChute in the PowerChute Setup wizard.

Enable HPE SimpliVity Support

To enable HPE SimpliVity support, open the PowerChute Setup wizard and follow the steps below.

  1. Select HPE SimpliVity from the Hyperconverged Infrastructure Support drop-down list in the vCenter Server Details screen and click Next.
  1. In the HPE SimpliVity Details screen, enter your HPE SimpliVity credentials to connect to your Cluster. The default user name is "svtcli", and it is not recommended to change this.
  2. Click Next to validate the connection.
  3. If the connection to your HPE SimpliVity Cluster is successful, you will be directed to the Virtualization Settings screen where you can configure your HPE SimpliVity settings. These settings can later be edited in the Virtualization Settings screen in the PowerChute UI.

HPE SimpliVity Virtualization Settings

When HPE SimpliVity support is enabled, the OmniStack Virtual Controller Shutdown/Startup section will appear in the Virtualization Settings screen in the PowerChute UI.