The events below are non-configurable and relate to virtualization tasks such as VM shutdown.
|
|
Click an event below for more information. |
A critical event has occurred on the UPS powering the Nutanix Cluster and PowerChute is shutting down the Acropolis File Server (AFS) VMs in the Cluster.
PowerChute was unable to shut down the Acropolis File Server (AFS) VMs in the Cluster.
A critical event has been resolved and PowerChute is trying to start up the Acropolis File Server (AFS) VMs in the Cluster.
PowerChute was unable to start up the Acropolis File Server (AFS) VMs in the Cluster.
PowerChute did not detect any active replications for a Protection Domain. This step of the shutdown sequence is skipped, and PowerChute continues to the next step, shutting down the Nutanix Cluster.
PowerChute detected active replications for a Protection Domain. PowerChute will wait the delay specified in the Duration field on the Protection Domain Settings screen before aborting replications.
PowerChute is aborting any active replications of your protection domain.
PowerChute was unable to abort your active protection domain replications.
PowerChute starts a maintenance mode task on the host when a critical UPS event occurs.
PowerChute is attempting to disable Metro Availability.
PowerChute could not disable Metro Availability on the Nutanix Cluster.
PowerChute is attempting to enable Metro Availability.
PowerChute starts a maintenance mode task on the host when a critical UPS event occurs.
PowerChute could not enable Metro Availability on the Nutanix Cluster.
PowerChute was unable to stop the cluster services.
An authentication error occurred when connecting to the cluster.
Some active replications could not be aborted.
The cluster service is not running. Cluster stop operations can't be executed.
The cluster stop operation was executed but the cluster is still running after the configured duration elapsed.
Authentication failures occurred when connecting to the cluster controller VMs for the cluster stop operation.
PowerChute could not connect to any cluster controller VM during the cluster stop operation.
The time required for the AFS stop operation exceeded the configured duration.
An error occurred when stopping AFS.
The cluster service did not start within the configured duration.