Protection Domain Settings

A protection domain is a collection of VMs that are backed up or replicated on a schedule to recover data. The Abort Active Replications checkbox is selected by default, and this option should be selected if your protection domain is configured to replicate on a schedule.

If enabled, PowerChute will wait the time specified in the Duration field before aborting any active protection domain replications in the event of a critical UPS event.

NOTE: The Duration field will only be taken into consideration if there are active replications when PowerChute reaches this step in the shutdown sequence. If there are no active replications this duration will not be included in the shutdown sequence.

Metro Availability spans a datastore across two sites (local and remote) and synchronously replicates data between the two sites. If the Disable Metro Availability checkbox is selected, Metro Availability will be deactivated in the event of a shutdown. This option should be selected if Metro Availability is configured on your Cluster.

Protection Domain Settings