If you have a Dell VxRail Cluster with ESXi as your hypervisor, you can enable Dell VxRail support for PowerChute in the PowerChute Setup wizard.
|
|
Dell VxRail support is available with the Network Management Card 3. Please refer to the Operating System and Compatibility Chart for the supported NMC 3 firmware version number. |
|
|
It is not supported to select HTTP as the communication protocol to communicate with the NMC for Dell VxRail configuration. HTTPS must be selected. |
When attempting to connect to VxRail Manager, if an untrusted SSL certificate is detected, a dialog to view the certificate will appear. Please verify that the certificate is correct and accept it in order to proceed. The certificate will be added to the PowerChute-keystore.
To enable Dell VxRail support, open the PowerChute Setup wizard and follow the steps below.
|
|
NOTES:
|
Click Next to validate the connection.
When Dell VxRail support is enabled, an additional section will appear in the Virtualization Settings screen in the PowerChute UI. For more information on this section, see: