For Single and Redundant and Parallel UPS configurations, the IP address of each NMC that PowerChute is communicating with is displayed under the UPS Configuration menu option.
For Advanced UPS configuration, each UPS Setup is displayed as a menu item and the IP address of the NMC(s) with which PowerChute is communicating is displayed under each UPS setup.
Click on the IP address to view the UPS information specific to that NMC. If the NMC has VMware Hosts associated with it, you can edit these settings for a specific NMC on this page. This overrides the global NMC settings configured via the initial PowerChute Setup or via the Shutdown Settings screen.
UPS information displayed includes:
The NMC Host Name from the NMC's DNS settings page under Network - DNS - Configuration is also displayed. This is not the same as the UPS name that can be set under Configuration - UPS General on the NMC.
Clicking the Launch button opens the NMC user interface.