In this example, there are two VMware hosts, and a vCenter Server being powered by a single UPS. PowerChute is installed on the vCenter Server machine outside the cluster. Shutdown command files/SSH actions are configured to run after host shutdown. Delay Maintenance Mode is enabled, and VM Prioritization is enabled and VMs/vApps are prioritized into High, Medium, Low, Group 1, Group 2 priority groups.

The following shutdown sequence occurs when the shutdown action is enabled for the On Battery event.
PowerChute begins to shut down the VMs and vApps on VMware hosts A and B in the order in which they are prioritized:
First, the un-prioritized VMs/vApps are shut down sequentially. As the duration for un-prioritized VMs/vApps elapses, the Group 2 VMs/vApps are shut down, followed by Group 1 priority VMs/vApps, then Low priority VMs/vApps, and Medium priority VMs/vApps, and finally the High priority VMs/vApps are shut down. The VMs/vApps within each priority group are not shut down in a particular order.
In this example, a UPS device is powering the vCenter Server, and a single UPS is powering the two Nutanix hosts in the Cluster. PowerChute is installed on the vCenter Server machine and is monitoring all UPS devices. Shutdown command files/SSH actions are configured to run after host shutdown. Delay Maintenance Mode is enabled, and VM Prioritization is enabled and VMs/vApps are prioritized into High, Medium, Low, Group 1, Group 2 priority groups.

Critical event on UPS Group: Option to shut down virtual hosts is enabled for this UPS. VM Migration and VM Prioritization are enabled.
VMs/vApps will be shut down in the VM Shutdown sequence, in
the order in which they are prioritized:

First, the un-prioritized VMs/vApps are shut down sequentially. As
the duration for un-prioritized VMs/vApps elapses, the Group 2 VMs/vApps
are shut down, followed by Group 1 priority VMs/vApps, then Low priority
VMs/vApps, and Medium priority VMs/vApps, and finally the High priority
VMs/vApps are shut down. The VMs/vApps within each priority group
are not shut down in a particular order.
PowerChute shuts down Acropolis File Services.
PowerChute shuts down Host A and Host B.
PowerChute runs the shutdown command file or SSH action, if configured.
The UPS turns off after the shutdown time has elapsed.