VMware with HyperFlex Support: UPS without Outlet Groups

Example 1a: Turn off the UPS enabled, no shutdown command file or SSH action configured, internal vCenter Server Appliance, PowerChute on physical Windows machine.

PowerChute is installed on a physical machine outside the Cluster, configured for a Single/Redundant UPS configuration with 2 nodes in a Cluster. The option to Turn off the UPS is enabled on the Shutdown Settings page, Delay Host Maintenance Mode is enabled on the Virtualization Settings page. No shutdown command file or SSH action configured. The durations in this example are as follows:

When a critical UPS event, such as On Battery occurs, the following sequence is triggered.

  1. PowerChute reports that the UPS is on battery.
  2. After the shutdown delay configured for the On Battery event has elapsed, PowerChute issues a command to turn off the UPS. UPS turnoff starts.
  3. PowerChute starts to shut down User VMs and vApps.
  4. After 2 minutes (VM/vApp Shutdown Delay), PowerChute shuts down the vCenter Server Appliance.
  5. After 240 seconds (vCSA Shutdown Delay), PowerChute shuts down the HyperFlex Cluster.
  6. After 180 seconds (Cluster Shutdown Delay), PowerChute issues a command to shut down the Controller VMs.
  7. After 120 seconds (Controller VM Shutdown Delay), the VMware Hosts enter maintenance mode and are shut down sequentially if all VMs are powered off, otherwise the maintenance mode task is cancelled. The delay between placing each host into maintenance mode is the value set for Delay Maintenance Mode (30 seconds).
  8. After a 70 second delay, the operating system on the physical machine running PowerChute starts to shut down.
  9. The UPS will wait the amount of time indicated by one of the following, whichever is greater:

Low Battery Duration or Maximum Required Delay
These are shown on the Configuration - Shutdown page in the NMC interface.

  1. After this delay, a further non-configurable two minute delay is counted down.
  2. The UPS will then turn off after the user-configurable Shutdown Delay time has elapsed.
    This is configurable on the Configuration - Shutdown page in the NMC user interface.

It is recommended that the  Low Battery Duration is configured to allow enough time for the Operating System shutdown to complete. Ideally the operating system should have shut down before the non-configurable two minute delay (step 10) starts to count down.

Example 1b: Turn off the UPS enabled, no shutdown command file or SSH action configured, external vCenter Server Appliance, PowerChute deployed as a VM.

PowerChute is deployed as VM inside the Cluster, configured for a Single/Redundant UPS configuration with 2 nodes in a Cluster. HA is enabled on the Cluster and there is an external vCenter Server Appliance. The option to Turn off the UPS is enabled on the Shutdown Settings page, Delay Host Maintenance Mode is enabled on the Virtualization Settings page. No shutdown command file or SSH action configured. The durations in this example are as follows:

When a critical UPS event, such as On Battery occurs, the following sequence is triggered.

  1. PowerChute reports that the UPS is on battery.
  2. After the shutdown delay configured for the On Battery event has elapsed, PowerChute issues a command to turn off the UPS. UPS turnoff starts.
  3. PowerChute starts to shut down User VMs and vApps.
  4. After 2 minutes (VM/vApp Shutdown Delay), PowerChute shuts down the HyperFlex Cluster.
  5. After 180 seconds (Cluster Shutdown Delay), PowerChute issues a command to shut down the Controller VMs.
  6. After 120 seconds (Controller VM Shutdown Delay), the VMware Hosts enter maintenance mode and are shut down sequentially if all VMs are powered off, otherwise the maintenance mode task is cancelled. The delay between placing each host into maintenance mode is the value set for Delay Maintenance Mode (30 seconds). The PowerChute host is powered off last.
  7. The UPS will wait the amount of time indicated by one of the following, whichever is greater:Low Battery Duration or Maximum Required Delay
    These are shown on the Configuration - Shutdown page in the NMC interface.
  8. After this delay, a further non-configurable two minute delay is counted down.
  9. The UPS will then turn off after the user-configurable Shutdown Delay time has elapsed.
    This is configurable on the Configuration - Shutdown page in the NMC user interface.

It is recommended that the Low Battery Duration is configured to allow enough time for the Operating System shutdown to complete.

Example 2a: Turn off the UPS enabled, shutdown command file configured, internal vCenter Server Appliance, PowerChute on physical Windows machine.

PowerChute is installed on a physical machine outside the Cluster, configured for a Single/Redundant UPS configuration with 2 nodes in a Cluster. The option to Turn off the UPS is enabled on the Shutdown Settings page, Delay Host Maintenance Mode is enabled on the Virtualization Settings page. A shutdown command file is configured. The durations in this example are as follows:

When a critical UPS event, such as On Battery occurs, the following sequence is triggered.

  1. PowerChute reports that the UPS is on battery.
  2. After the shutdown delay configured for the On Battery event has elapsed, PowerChute issues a command to turn off the UPS. UPS turnoff starts.
  3. PowerChute starts to shut down User VMs and vApps.
  4. After 2 minutes (VM/vApp Shutdown Duration), PowerChute shuts down the vCenter Server Appliance.
  5. After 240 seconds (vCSA Shutdown Duration), PowerChute shuts down the HyperFlex Cluster.
  6. After 180 seconds (Cluster Shutdown Duration), PowerChute issues a command to shut down the Controller VMs.
  7. After 120 seconds (Controller VM Shutdown Delay), PowerChute starts to execute the shutdown command file.
  8. After the delay configured for the command file has elapsed, the VMware Hosts enter maintenance mode and are shut down sequentially if all VMs are powered off, otherwise the maintenance mode task is cancelled. The delay between placing each host into maintenance mode is the value set for Delay Maintenance Mode (30 seconds).
  9. After a 70 second delay, the operating system on the physical machine running PowerChute starts to shut down.
  10. The UPS will wait the amount of time indicated by one of the following, whichever is greater:Low Battery Duration or Maximum Required Delay.
    These are shown on the Configuration - Shutdown page in the NMC interface.
  11. After this delay, a further non-configurable two minute delay is counted down.
  12. The UPS will then turn off after the user-configurable Shutdown Delay time has elapsed.
    This is configurable on the Configuration - Shutdown page in the NMC user interface.

It is recommended that the Low Battery Duration is configured to allow enough time for the Operating System shutdown to complete. Ideally the operating system should have shut down before the non-configurable two minute delay (step 11) starts to count down.

Example 2b: Turn off the UPS enabled, shutdown command file configured, external vCenter Server Appliance, PowerChute deployed as a VM.

PowerChute is deployed as VM inside the Cluster, configured for a Single/Redundant UPS configuration with 2 nodes in a Cluster. HA is enabled on the Cluster and there is an external vCenter Server Appliance. The option to Turn off the UPS is enabled on the Shutdown Settings page, Delay Host Maintenance Mode is enabled on the Virtualization Settings page. A shutdown command file is configured. The durations in this example are as follows:

When a critical UPS event, such as On Battery occurs, the following sequence is triggered.

  1. PowerChute reports that the UPS is on battery.
  2. After the shutdown delay configured for the On Battery event has elapsed, PowerChute issues a command to turn off the UPS. UPS turnoff starts.
  3. PowerChute starts to shut down User VMs and vApps.
  4. After 2 minutes (VM/vApp Shutdown Duration), PowerChute shuts down the HyperFlex Cluster.
  5. After 180 seconds (Cluster Shutdown Duration), PowerChute issues a command to shut down the Controller VMs.
  6. After 120 seconds (Controller VM Shutdown Delay), PowerChute starts to execute the shutdown command file.
  7. After the delay configured for the command file has elapsed, the VMware Hosts enter maintenance mode and are shut down sequentially if all VMs are powered off, otherwise the maintenance mode task is cancelled. The delay between placing each host into maintenance mode is the value set for Delay Maintenance Mode (30 seconds). The PowerChute host is powered off last.
  8. The UPS will wait the amount of time indicated by one of the following, whichever is greater:Low Battery Duration or Maximum Required Delay.
    These are shown on the Configuration - Shutdown page in the NMC interface.
  9. After this delay, a further non-configurable two minute delay is counted down.
  10. The UPS will then turn off after the user-configurable Shutdown Delay time has elapsed.
    This is configurable on the Configuration - Shutdown page in the NMC user interface.

It is recommended that the Low Battery Duration is configured to allow enough time for the Operating System shutdown to complete.

Example 3a: Turn off the UPS enabled, shutdown command file configured, Execute Command File after Host Shutdown enabled, internal vCenter Server Appliance, PowerChute on physical Windows machine.

PowerChute is installed on a physical machine outside the Cluster, configured for a Single/Redundant UPS configuration with 2 nodes in a Cluster. The option to Turn off the UPS is enabled on the Shutdown Settings page, Delay Host Maintenance Mode is enabled on the Virtualization Settings page. A shutdown command file is configured. Execute Command File after Host Shutdown is enabled, with a delay of 30 seconds applied. The durations in this example are as follows:

When a critical UPS event, such as On Battery occurs, the following sequence is triggered.

  1. PowerChute reports that the UPS is on battery.
  2. After the shutdown delay configured for the On Battery event has elapsed, PowerChute issues a command to turn off the UPS. UPS turnoff starts.
  3. PowerChute starts to shut down User VMs and vApps.
  4. After 2 minutes (VM/vApp Shutdown Duration), PowerChute shuts down the vCenter Server Appliance.
  5. After 240 seconds (vCSA Shutdown Duration), PowerChute shuts down the HyperFlex Cluster.
  6. After 180 seconds (Cluster Shutdown Duration), PowerChute issues a command to shut down Controller VMs.
  7. After 120 seconds (Controller VM Shutdown Duration), the VMware Hosts enter maintenance mode and are shut down sequentially if all VMs are powered off, otherwise the maintenance mode task is cancelled. The delay between placing each host into maintenance mode is the value set for Delay Maintenance Mode (30 seconds).
  8. Following the 30 second delay configured for the Execute Command File after Host Shutdown option, PowerChute starts to execute the shutdown command file.
  9. After the duration configured for the shutdown command file has elapsed, the OS Shutdown Command is issued and an additional 70 second delay is counted down before the operating system on the physical machine running PowerChute starts to shut down.
  10. The UPS will wait the amount of time indicated by one of the following, whichever is greater:Low Battery Duration or Maximum Required Delay.
    These are shown on the Configuration - Shutdown page in the NMC interface.
  11. After this delay, a further non-configurable two minute delay is counted down.
  12. The UPS will then turn off after the user-configurable Shutdown Delay time has elapsed.
    This is configurable on the Configuration - Shutdown page in the NMC user interface.

It is recommended that the Low Battery Duration is configured to allow enough time for the Operating System shutdown to complete. Ideally the operating system should have shut down before the non-configurable two minute delay (step 11) starts to count down.

Example 3b: Turn off the UPS enabled, SSH action configured, external vCenter Server Appliance, PowerChute deployed as a VM.

PowerChute is deployed as VM inside the Cluster, configured for a Single/Redundant UPS configuration with 2 nodes in a Cluster. HA is enabled on the Cluster and there is an external vCenter Server Appliance. The option to Turn off the UPS is enabled on the Shutdown Settings page, Delay Host Maintenance Mode is enabled on the Virtualization Settings page. A SSH action is configured to execute before host shutdown, with a delay of 30 seconds applied. The durations in this example are as follows:

When a critical UPS event, such as On Battery occurs, the following sequence is triggered.

  1. PowerChute reports that the UPS is on battery.
  2. After the shutdown delay configured for the On Battery event has elapsed, PowerChute issues a command to turn off the UPS. UPS turnoff starts.
  3. PowerChute starts to shut down User VMs and vApps.
  4. After 2 minutes (VM/vApp Shutdown Duration), PowerChute shuts down the HyperFlex Cluster.
  5. After 180 seconds (Cluster Shutdown Duration), PowerChute issues a command to shut down Controller VMs.
  6. After 120 seconds (Controller VM Shutdown Duration), PowerChute waits the 30 second delay configured for Execute SSH Action before Host Shutdown, and starts to execute the SSH action.
  7. VMware Hosts enter maintenance mode and are shut down sequentially if all VMs are powered off, otherwise the maintenance mode task is cancelled. The delay between placing each host into maintenance mode is the value set for Delay Maintenance Mode (30 seconds). The PowerChute host is powered off last.
  8. The UPS will wait the amount of time indicated by one of the following, whichever is greater:Low Battery Duration or Maximum Required Delay.
    These are shown on the Configuration - Shutdown page in the NMC interface.
  9. After this delay, a further non-configurable two minute delay is counted down.
  10. The UPS will then turn off after the user-configurable Shutdown Delay time has elapsed.
    This is configurable on the Configuration - Shutdown page in the NMC user interface.

It is recommended that the Low Battery Duration is configured to allow enough time for the Operating System shutdown to complete.