The following scenarios provide examples of how PowerChute and the UPS behave when a shutdown sequence is triggered.
VMware: UPS without Outlet Groups
VMware: UPS with Outlet Groups
VMware with Nutanix Support: UPS without Outlet Groups
VMware with Nutanix Support: UPS with Outlet Groups
VMware with HPE SimpliVity Support: UPS without Outlet Groups
VMware with HPE SimpliVity Support: UPS with Outlet Groups
VMware with HyperFlex Support: UPS without Outlet Groups
VMware with HyperFlex Support: UPS with Outlet Groups
VMware with Dell VxRail Support: UPS without Outlet Groups
VMware with Dell VxRail Support: UPS with Outlet Groups
VMware Shutdown - Single UPS Configuration
VMware Shutdown - HA Cluster
VMware Shutdown - vSAN Cluster
VMware Shutdown - Advanced UPS Configuration
VMware Shutdown - VM Prioritization
VMware with Nutanix Support: VM Prioritization
VMware with HPE SimpliVity Support: VM Prioritization
VMware with HyperFlex Support: VM Prioritization
VMware with Dell VxRail Support: VM Prioritization
Nutanix AHV: UPS without Outlet Groups
Nutanix AHV: UPS with Outlet Groups
Nutanix AHV Shutdown - Single UPS Configuration
Nutanix AHV Shutdown - Advanced UPS Configuration
Nutanix Shutdown - VM Prioritization
Hyper-V: UPS without Outlet Groups
Hyper-V: UPS with Outlet Groups
Hyper-V Shutdown - Single UPS Configuration
Hyper-V Shutdown - Advanced UPS Configuration
SCVMM: UPS without Outlet Groups
SCVMM: UPS with Outlet Groups
SCVMM Shutdown - Single UPS Configuration
SCVMM - Advanced UPS Configuration