SNMPv3 Configuration
Select Enable SNMPv3 access to configure
the SNMPv3 settings. Select Add Profile and
configure:
- User Name: In SNMPv3, all GET and SET
requests and SNMP Traps are matched to a user profile by the User
Name. Enter a user name of a length less than or equal to 32 ASCII
characters.
- Authentication Protocol: Select MD5,
SHA-1 or SHA-2 (SHA256 or SHA512) protocol. It is recommended to use
an SHA-2 protocol, if the NMS supports it.

|
It is not recommended to use the MD5 protocol. |
- Authentication Passphrase: Enter an
authentication password for the protocol selected, of 8-32 ASCII characters.
- Privacy Protocol: Select AES-128, AES-192*,
AES-192 Ex†, AES-256* , AES-256 Ex†,
or DES. It is recommended to use the AES-256 protocol, if the NMS
and PowerChute JRE support it.
- Privacy Passphrase: Enter a privacy
password for the encryption protocol selected, of 8-32 ASCII characters.
- Access Type:
- Disable:
No SNMP GET or SET requests are permitted.
- Read:
Only SNMP GET requests are permitted.
- Read/Write:
SNMP GET and SET requests are permitted.
To edit an existing SNMPv3 user profile, click the
button. To delete an SNMPv3
user profile, click the
button.
Click Apply to save the SNMPv3 configuration.

|
Certain Network Management
Systems require the SNMP Engine ID to communicate via SNMP. The
SNMP Engine ID is
displayed on the SNMP Settings page of the PowerChute user interface. |