Protection Domain Settings

A protection domain is a collection of VMs that are backed up or replicated on a schedule to recover data. The Abort Active Replications checkbox is enabled by default, and this option should be enabled if your protection domain is configured to replicate on a schedule.

If enabled, PowerChute will wait the time specified in the Duration field before aborting any active protection domain replications in the event of a critical UPS event.

NOTE: The Duration field will only be taken into consideration if there are active replications when PowerChute reaches this step in the shutdown sequence. If there are no active replications this duration will not be included in the shutdown sequence.

Protection Domain Settings