Virtualization Settings

Virtual machine (VM) settings like VM Shutdown, Controller VM Shutdown, and Cluster Shutdown can be configured in the Virtualization Settings screen.

Virtualization Settings

For more information see:

Virtualization Settings in Advanced UPS Configuration

In an advanced UPS configuration, settings entered on this page will be applied to all UPS Setups if the Apply Virtualization Settings to all UPS Setups checkbox is selected. This checkbox is enabled by default.

If you have applied settings to individual UPS Setups, you should uncheck this option to prevent them from being overwritten.

Individual UPS Setup Settings applied