Nutanix Host Protection

Once connected to the Nutanix Cluster, PowerChute displays all of the Nutanix hosts in the inventory in a tree view. From this screen you can select the hosts that PowerChute should protect.

Single, Redundant, and Parallel-UPS configurations

Specify the hosts in the left-hand panel you want to protect by dragging them to the right-hand panel of this screen. Each host listed in the left-hand panel must be added to the right-hand panel of this screen before you can proceed with your configuration.

When a critical UPS event occurs, PowerChute will shut down hosts in the order that they appear in the right-hand panel. You can change this order by clicking on a host in the right-hand panel and dragging it up and down.

Advanced UPS configuration

Advanced UPS configuration

In an advanced UPS configuration, the Nutanix hosts are powered separately by one or more UPS device(s) in a UPS Setup. The right-hand panel shows the UPS Setups that have been configured and are monitored by PowerChute. You need to associate each Nutanix host in the left-hand panel with the UPS by which it is powered. To do this, drag each host to the UPS/UPS group in the right-hand panel.

In an advanced UPS configuration, all hosts in the Nutanix Cluster must be protected by the same UPS or UPS group.

For this configuration, PowerChute must be installed on a physical Windows machine outside the Cluster.

If the IP address/Hostname of any of the hosts are changed, it will be necessary to re-associate the hosts with the UPS devices.

 

Physical UPS Setup Power Protection

In Advanced UPS Setups, PowerChute can monitor UPS devices which are powering equipment outside a Nutanix Cluster (e.g. a Storage Array Device or a physical server machine running PowerChute).

For more information see Shutdown Settings for Advanced UPS Setups.

On the Host Protection page, do not link Nutanix hosts with the UPS devices that are powering the physical equipment.

 

The following additional options will then be displayed on the Shutdown Settings page:

 

PowerChute User Interface - Configure Shutdown Conditions

PowerChute Setup - Configure Shutdown Conditions