In a Hyper-V configuration, you have the option to stop the cluster as part of the shutdown sequence. If the Enable Stop Cluster checkbox is enabled, PowerChute will stop your Hyper-V cluster after VMs are migrated and shut down, and before the PowerChute operating system is shut down. See also: Hyper-V Failover Cluster with Cluster Stop and VM Migration

|
|
Using the Shutdown Duration field, ensure that you allow sufficient time for your cluster to stop. |
The time specified in the Startup Duration field is the time PowerChute will wait before re-starting your cluster once a UPS critical event has been resolved.