Free/Open Source License Details

PowerChute stores the details of the free and open source licenses used in PowerChute in the notice.txt file located in the PowerChute installation directory. If the default installation directory was chosen during installation, this location will be:

  1. C:\Program Files\APC\PowerChute for Windows systems

  2. /opt/APC/PowerChute for Linux systems