The events below are non-configurable and relate to virtualization tasks carried out when shutting down a HPE SimpliVity cluster.
|
|
Click an event below for more information. |
A critical event has occurred on the UPS powering the Cluster and PowerChute is shutting down the OmniStack Virtual Controller [OVC] running the Cluster. The OmniStack Virtual Controller is shut down after all other VMs in the Cluster.
PowerChute was unable to gracefully shut down OmniStack Virtual Controller [OVC].
PowerChute was unable to shut down the OmniStack Virtual Controller [OVC] as insufficient time was provided in the OVC Shutdown Duration field.
A critical event has been resolved and PowerChute is attempting to start the OmniStack Virtual Controller [OVC]. This event is triggered after the host is online.
PowerChute was unable to start the OmniStack Virtual Controller [OVC].
Authentication errors occurred when connecting to the cluster OVCs.
A connection error occurred when connection to the cluster OVCs.