|
|
Click an event below for more information. |
A critical event has occurred on a UPS associated with this host. This will trigger a shutdown sequence.
The previously logged critical event has been resolved.
A critical event has occurred and PowerChute is attempting to start Maintenance mode on the host affected.
A critical event has occurred and PowerChute is attempting to start Maintenance mode on multiple hosts. This event is triggered when a critical event occurs on multiple hosts at the same time.
PowerChute has successfully started maintenance mode on a host. This event is logged for each host on which the event occurs.
PowerChute has stopped maintenance mode on a host. This event is logged for each host on which the event occurs.
The host on which PowerChute is attempting to start Maintenance mode is already in Maintenance mode. This event is logged for each host on which the event occurs.
The host on which PowerChute is attempting to stop Maintenance mode is not currently in Maintenance mode. This event is logged for each host on which the event occurs.
PowerChute has not successfully started Maintenance Mode on a host. This event is logged for each host on which the event occurs.
PowerChute is attempting to shut down the host via SCVMM. This event is logged for each host on which the event occurs.
PowerChute has successfully shutdown the host. This event is logged for each host on which the event occurs.
PowerChute shutdown of the host was not successful. This event is logged for each host on which the event occurs.