|
|
Click an event below for more information. |
There have been three invalid login attempts from a machine with the IP address listed in the event. Further login attempts will be prevented from this machine for two minutes. This is a security measure designed to prevent brute-force login attempts.
The Username has been changed by the user at the specified IP address. This is a security feature to notify the user when the Username has been changed.
The password has been changed by the user at the specified IP address. This is a security feature to notify the user when the password has been changed.
The authentication phrase has been changed by the user at the specified IP address. This is a security feature to notify the user when the authentication phrase has been changed.
The runtime remaining on the UPS has dropped below the Low battery duration value while the UPS was on battery.
A graceful shutdown command has been issued to the UPS using the NMC User Interface, the LCD display or by PowerChute. This event is logged for all UPS Configurations.
The PowerChute Web service has been started.
The operating system has started to shut down in response to
a critical UPS event.
The outlet group that PowerChute is registered with is turned off. This can indicate that PowerChute is not configured for the correct outlet group.
The outlet group that PowerChute is registered with is shutting down. A shutdown sequence will be started as a result.
If PowerChute was not registered with an Outlet group during setup it will be automatically registered with the first outlet group on the UPS by default.
PowerChute uses TCP ports 3052 and 6547 for the Web User Interface. This event will be logged if another application is already using either of the above ports.
Use the netstat command to identify which process is using these ports or change the values using the PowerChute Configuration File.
PowerChute has begun to open the port it requires for the Web UI.
PowerChute has successfully opened the port it requires for the Web UI.
PowerChute uses UDP port 3052 for communication with the NMC. This event will be logged if another application is already using this port. Use the netstat command to identify which application is using the port. This port cannot be changed.
PowerChute has begun to open the port required for NMC communications.
PowerChute was able to open the port it needs for NMC communications.
Reported when the PowerChute Agent cannot communicate with the Network Management Card over the network. This could be due to a mismatch in security credentials or a network issue.
Reported when the Network Management Card cannot communicate with the UPS. If this issue persists please contact technical support.
This can occur if registering with an NMC that has HTTPS enabled and is using an SSL certificate that is not signed by a trusted root certification authority.
Ensure that trusted certificates are added to the PowerChute-keystore during registration. See Certificate Management for more information.
Occurs when registering with an NMC that has HTTPS enabled if the SSL cert is not signed by a trusted root certification authority.
PowerChute added an NMC SSL certificate to the PowerChute-keystore. See Certificate Management for more information.
Reported when one UPS goes on battery in a UPS configuration with multiple UPS's.
Reported when one UPS in a UPS configuration with multiple UPS's returns to On Line operation.
The advanced option is enabled under UPS Shutdown Settings for a Redundant UPS Configuration and one UPS is on Battery.
Reported when one UPS turns off in a UPS configuration with multiple UPS's.
Reported when one UPS turns back on in a UPS configuration with multiple UPS's.
Reported in a Redundant UPS Configuration.
In n+1 redundancy, this is reported when 2 UPS's turn off.
In n+2 redundancy, this is reported when 3 UPS's turn off.
In n+3 redundancy, this is reported when 4 UPS's turn off.
Reported in a Redundant UPS Configuration.
In n+1 redundancy, this is reported when 2 UPS's turn off.
In n+2 redundancy, this is reported when 3 UPS's turn off.
In n+3 redundancy, this is reported when 4 UPS's turn off.
This occurs in a Redundant or Parallel-Redundant UPS Configuration when two different critical UPS events are active.
One of the UPS devices in a Parallel-UPS configuration has been removed from the Parallel system.
PowerChute has sent a graceful shutdown command to the UPS. This is logged when a critical event occurs and the option to Turn off the UPS is enabled on the Shutdown settings page.
PowerChute has sent a graceful shutdown command to the UPS Outlet group. This is logged when a critical event occurs and the option to Turn off the UPS Outlet Group is enabled on the Shutdown settings page.
A new user has connected to PowerChute via SNMP. This event is logged the first time a user connects after the PowerChute service restarts, or a SNMP setting is changed.
PowerChute detected a new user attempting to connect via SNMP. This event is logged the first time a user is unable to connect after the PowerChute service restarts, or a SNMP setting is changed.
NOTE: Some SNMP managers make unsuccessful attempts as part of their connection process. This will be indicated by the user "initial".
A PowerChute setting has been changed by [User] via SNMP.