The events below are non-configurable and relate to virtualization tasks such as cluster shutdown. The events listed here are common across the hyperconverged infrastructure (HCI) environments: Nutanix, HPE SimpliVity, and HyperFlex.
|
|
Click an event below for more information. |
PowerChute is attempting to shut down the Cluster.
PowerChute successfully shut down the Cluster.
PowerChute was unable to shut down the Cluster.
PowerChute is attempting to start up the Cluster.
PowerChute successfully started up the Cluster.
PowerChute was unable to start up the Cluster.
A critical event has occurred on the UPS powering the Cluster and PowerChute is shutting down all Controller Virtual Machines in the Cluster. Controller VMs are shut down after all other VMs in the Cluster, and the Cluster itself are shut down.
A critical event has been resolved and PowerChute is attempting to start up the Controller Virtual Machine [CVM]. This event is triggered after the host is online.
PowerChute was unable to gracefully shut down Controller VM [CVM].
A critical event has been resolved and PowerChute is waiting for the Controller Virtual Machines in the Cluster to startup. The Cluster will start up when Controller VM startup is complete.
vCLS shutdown was skipped due to insufficient user privileges or because vCLS is already disabled.