The events below are non-configurable and relate to virtualization tasks carried out when shutting down a HyperFlex cluster.
|
|
Click an event below for more information. |
PowerChute cannot establish a connection with the HyperFlex Rest service and may not be able to perform cluster operations.
PowerChute could not shut down the cluster within the Shutdown Duration specified. PowerChute will wait for the Shutdown Duration to elapse before attempting to shut down the cluster again with respect to the cluster_ops_retries value in the PowerChute configuration file. For more information, see Cluster Shutdown/Startup.
PowerChute could not start the cluster within the Startup Duration specified. PowerChute will wait for the Startup Duration to elapse before attempting to start the cluster again with respect to the cluster_ops_retries value in the PowerChute configuration file. For more information, see Cluster Shutdown/Startup.
The cluster stop operation did not complete within the configured duration.
The cluster did not start within the configured duration.