|
|
Click an event below for more information. |
A critical event has occurred on a UPS associated with this host. This will trigger a shutdown sequence.
The previously logged critical event has been resolved.
A critical event has occurred and PowerChute is trying to migrate virtual machines to another host.
A critical event has occurred and PowerChute is trying to shut down virtual machines.
A critical event has been resolved or a host has restarted, and PowerChute is trying to start up the VMs on that host.
PowerChute is reattempting to power on VMs following an unsuccessful attempt.
Before trying to migrate or shut down virtual machines (see
events above), PowerChute suspends the hosts.
This prevents other VMs getting powered on or migrated to this
host while a critical event is active.
Before shutting down the operating system, PowerChute resumes
the node in the failover cluster.
This ensures the integrity of the cluster and that all services
will be available when the OS is subsequently powered on.
The cluster node cannot be resumed.
A critical event has occurred and PowerChute is trying to stop the cluster. This is the second last step in the shutdown sequence, and occurs after VMs are migrated and shut down, and before the PowerChute operating system is shut down.
PowerChute was unable to stop the cluster.
A critical event has been resolved, and PowerChute is trying to start up the cluster.
The cluster cannot be re-started.