Event Configuration

 

When UPS events occur, PowerChute can be configured to log the event, notify users, execute a command file or initiate a system shutdown through the Configure Events screen.

The checked.jpg symbol indicates that the action is enabled for this event while the check_circle.jpg symbol indicates that the action is not enabled.

Descriptions of events are in the PowerChute Events and Logging sections.