|
V3.62 LARGE : TLXCDLUOFS36 TLXCDLTOFS36 TLXCDLFOFS36 |
|||
![]() |
OPC Factory Server V3.62 3303 SP1 |
||
Copyright © 2003-2019 Schneider Electric Industries SAS
Enhancements - Bug Fixing :
| 3303 SP1 |
Bug fixing : A crash may occur when IOPCAsyncIO2::Refresh is performed concurrently to IOPCItemMgt::RemoveItems Bug fixing : A hang may occur when activating items with IOPCItemMgt::SetActiveState or IOPCItemMgt::AddItems is performed concurrently to IOPCItemMgt::RemoveItems |
| Bug fixing : A hang may occur on communication timeout when PLC link redundancy is configured. | |
| Bug fixing : The PLC link redundancy switch may be not performed if Address1 and Address 2 never got a common online status | |
| Bug fixing : On EcoStruxure Control Expert build change, Program Units items populated with XVM symbol link were discarded | |
| Bug fixing : Write operation on array of items postfixed with ";s" was badly performed if the item had not VT_UI1 type (for instance myAlias!%MW10:4;s) | |
| Bug fixing : Activation of a pending or missing license may fail. | |
| Bug fixing : The diagnostics window may not log new information after overflow was mitigated. | |
| Bug fixing : The Configuration tool Device Address Wizard did not show PL7, XTEL and ORPHEE PLC types. | |
| Bug fixing : A same item activated several times may miss an activation after a data dictionary update. | |
| Bug fixing : Unlocated items accessed with PRJ Concept link may fail. | |