Last revision: 12/5/2023
Ecostruxure Machine SCADA Expert and AVEVA System Platform both use Industrial Graphics. Because of this, Ecostruxure Machine SCADA Expert 2020 SP3 can only coexist with AVEVA System Platform 2020 R2 SP1 and AVEVA System Platform 2020 R2 SP1 Patch 01.
This is a summary of important features and enhancements that have been introduced in this version.
We added or significantly improved the following communication drivers in this release:
Driver |
Description |
---|---|
IE104 |
Communication with devices using the IEC 60870-5-104 protocol. This driver has been enhanced to allow the user to communicate with multiple Common addresses in the station field for the same driver instance.
|
ABCIP |
Communication with Allen-Bradley Common Industrial Protocol (CIP) over Ethernet/IP for ControlLogix, FlexLogix, CompactLogix, and MicroLogix controllers. Driver enhancements:
|
COSYS |
TCP/IP and Serial Communication using PLC Handler CodeSys Library. Driver enhancements:
|
DNP |
Communication with devices using the DNP3 protocol. Improved reconnection logic and reduced the occurrence of timeouts.
|
MITSU |
Communication with Mitsubishi FX Series devices. This driver now supports TCP/IP and Serial Communication for the Linux runtime.
|
MQTT |
Communication with devices that support Message Queuing Telemetry Transport (MQTT) protocol. Driver enhancements:
|
OMDIR |
Communication with OMRON controllers compatible with the Ethernet/IP CIP protocol that supports symbolic addressing. Support for this driver has been added for Windows and Linux runtimes. Note: The OMDIR driver and its associated features are available only if you have purchased the appropriate license option.
|
TSAA |
Communication with Triconex devices using the TSAA protocol over UDP/IP. Driver enhancements:
|
For more information, see Issues Resolved for Specific Communication Drivers below.
We continue to improve our product security posture. In particular, we have done the following:
Updated Japanese-language messages and menus, improving readability.
Remote Agent for Linux runtimes has been upgraded. Follow these directions to install the update:
This is a summary of features that have been deprecated or removed from this version.
The Enable Enhanced Graphics option for Project Screens is now enabled and, in order to improve performance and security, the option to disable it has been removed. This feature provides anti-aliasing for lines, edges, gradient fills on Shapes, Text objects, and Button objects (with the exception of conical gradient fills). It also provides the ability to set opacity (Visibility property) for some screen objects. This feature is not supported in projects configured to run on the Embedded target platform.
In order to enhance project security, AutoCAD DXF files cannot be imported as linked external images.
In order to enhance security, NTWebServer has been removed from this release.
This is a list of important issues that have been resolved in this version.
These are issues that were reported by our users and then logged in our customer relationship management system. If you reported an issue to us, you should have been given a case number at that time. You can look for your case number in the list below.
Please note that documentation changes are not counted as resolved issues, so if you reported an issue and it was resolved by a documentation change (e.g., by clarifying a step in a procedure), then it might not be included in this list.
Case No. |
ID |
Description |
960017480 |
612603 |
SMTP email client did not support Transport Layer Security (TLS) 1.3. |
960055220 |
1135583 |
Only the first 50 or 100 characters of a String tag were saved when selecting the Retentive Value string tag property.
|
960060077 |
1101942 |
Log to File did not log Japanese characters. |
960072530 |
1231313 |
Viewer.exe module froze after changing a user password through the SetPassword() function. |
960074812 |
1504555 |
Mobile Access Alarm History object did not consistently update when a filter was applied through the Selection field of the Filters dialog.
|
960094239 |
1533421 |
The Trend Object loaded partial data after pausing from periods of time with more than 32000 points when using Local Time + Default Milliseconds.
|
960095919 |
1417914 |
Rotation animation was not working as expected for horizontal rectangles made out of the Closed Polygon shape. |
960098069 |
1421067 |
Trend Control objects in Mobile Access were unable to retrieve historical data when using custom properties. |
960098089 |
1497770 |
Database/ERP connections timed out after 30 seconds. |
960102034 |
1441093 |
Symbol Flip Horizontal or Flip Vertical would not persist after closing and reopening screen. |
960103901 |
1497309 |
Retentive tag values in Scheduler Worksheets were triggering a Tag Database popup when connecting to the runtime.
|
960105404 |
1486496 |
ShowMessageBox was not working as expected in Mobile Access. |
960107855 |
1503105 |
Insert field on DB/ERP worksheets was not working as expected with a large number of rows. |
960110646 |
1505880 |
Remove blank lines in project database in the Verify Project dialog was not removing blank lines when there were any fields filled in the tags database.
|
960110653 |
1506328 |
Adding rows to a CSV file during runtime using Grid Object Insert Trigger was adding additional carriage return characters.
|
960112075 |
1513940 |
Mobile Access threw an error "Fail to open Database" when connecting to SQL database with Data Protection enabled.
|
960112601 |
1543472 |
Secure Viewer intermittently failed to load the default user after an update. |
960112601 |
1803052 |
Secure Viewer screen focus was incorrect at runtime startup. |
960112904 |
1704166 |
Special characters in tags were not supported when using the built-in OPC UA Server. |
960112904 |
1606912 |
The OPC UA Client connection was generating a BadWaitingForInitialData error after a reconnection. |
960114001 |
1586978 |
OPC UA Tag Integration lost synchronization when the OPC Server was offline. |
960115021 |
1575466 |
Grid Objects using an ampersand in the database connection password were not publishing correctly in HTML. |
960122634 |
1593519 |
Industrial Graphics were not updating correctly after an ungraceful disconnection. |
960123268 |
1594527 |
OPC UA Client connections were not updating correctly to use the new connection format. |
960123981 |
1596903 |
Copied grouped objects were shifting position within the group. |
960129112 |
1632475 |
IDE reliability degraded after adding animation to a linked symbol. |
960134779 |
1655030 |
Enhanced Text Object and Animation Text Data Link resize feature in Mobile Access was applying the manually resized text to other text objects in the same screen.
|
960137039 |
1667655 |
Mobile Access Smart Message object tag values were not updating on tag value change. |
960137678 |
1673319 |
Could not connect to on-premises Historian using Database Gateway credentials instead of a user name and password. |
960137722 |
1682474 |
Mobile Access did not support the Binary Alarm History project setting. |
960139223 |
1678949 |
Invalid members were able to be added to Class Array tags without reporting an error. |
960139258 |
1682242 |
In applications running as a service, tags were not updating automatically. |
960139258 |
1678974 |
Verify Project was taking too long for large projects. |
960139548 |
1680335 |
Filter Expressions were not reading Time values correctly for Alarm/Event object Filters. |
960140147 |
1682414 |
OpcUaBrowseToJson() function was not documented. |
960141709 |
1716518 |
Mobile Access was stopping, even though STADOSVR and Studio manager were still running. |
960143272 |
1696302 |
PDFCreate() was not executing properly when executed twice within a small time window. |
960144651 |
1755384 |
Linked Picture objects were affecting Screen editing. |
960144975 |
1706529 |
Grouped objects were not maintaining their shapes when being rotated and copied. |
960144975 |
1797649 |
Groups of symbols were not keeping their original forms when close the screen edge. |
960146719 |
1711879 |
In Mobile Access, Alarm Worksheet numbers were being displayed in place of Alarm Group Names. |
960146820 |
1733012 |
Trend data objects with a TXT file data source and Sort selected were not displaying data consistently using different Durations.
|
960146950 |
1768671 |
Security System Group Account Advanced Password aging did not require a new password to replace the old password.
|
960149055 |
1730154 |
SetDisplayUnit() was not available for the Linux runtime and Mobile Access. |
960149993 |
1730450 |
1500 tag licenses were not enabled for Embedded HMI. |
960151585 |
1736280 |
Translation was not working for a Combo Box screen object using a database as Data Source. |
960152076 |
1738730 |
Trend worksheet created during runtime did not retain data after application restart. |
960152167 |
1738912 |
Any missing OPC UA node generated OPC UA Client errors and required application restart. |
960153665 |
1754668 |
The Verify Project "Remove blank lines in project database" option did not remove blank lines from class tags. |
960155356 |
1765311 |
Changing a service project's Startup Type caused an error. |
960155407 |
1774936 |
Tag properties of tags created in AVEVA Historian by Application Server were overwritten when the trend logger saved data in AVEVA Historian.
|
960156664 |
1768522 |
A project configured to run as a service was not able to be started from a Windows System Tray icon. |
960158055 |
1778192 |
OPC XML/DA Client did not read when ScanScreen was enabled on Mobile Access. |
960158965 |
1780003 |
Improved Industrial Graphics reliability. |
960161920 |
1801380 |
The screen scan mode on the Main Driver Sheet was working erratically. |
960163181 |
1803063 |
Hard-coded timeouts were causing Studio Database Gateway connection timeouts when connected to the Linux runtime.
|
960163839 |
1808877 |
"(Default Rights)" was a visible selection option when enabling the Security System "Display list of users at logon" option.
|
960164644 |
1814694 |
Supported and unsupported tags OPC UA were not documented. |
960164788 |
1809471 |
OPC UA was throwing COpcUaClientTask::OnDataChange exception. |
960153263 |
1756677 |
"Task Switch Enabled" feature was not included in the installation. |
960156175 |
1788461 |
Boolean tags were being overwritten on startup. |
960156544 |
1788047 |
Scheduled database queries were failing, sometimes halting the application. |
960165687 |
1861269 |
Saving screens with linked symbols caused IDE failure. |
960165931 |
1819262 |
Thin Client setup was missing dependencies. |
960172977 |
1859481 |
Class Array tags were not being validated in certain graphic screen objects. |
960177154 |
1874027 |
IDE performance degraded after opening the Object Finder in the Event Logger window. |
960177154 |
1874033 |
Tag Integration was causing the IDE to be unresponsive. |
960177204 |
1873964 |
There was no watchdog for OPC UA tag groups. |
960178652 |
1890614 |
GetSecuritySystemStatus() did not support redundant Active Directory servers. |
960178652 |
1906105 |
SetPassword() was failing. |
960180794 |
1895743 |
Combo box screen objects behaved inconsistently when the "Require confirmation" option was selected. |
960181070 |
1891886 |
OPC UA Tag integration was not working on Embedded HMI runtime. |
960182645 |
1896173 |
Opening a new application by double-clicking its APP file while another application was running opened the running application instead.
|
960182661 |
1896190 |
Large output logs degraded system performance. |
960185490 |
1913183 |
FileReadFields() was returning error "-3" when returning values to all array indexes. |
960186006 |
1913453 |
The CreateUser() function did not show the the complete list of available runtime groups in the Create User dialog in an Embedded HMI installation.
|
960186713 |
1924802 |
Alarm/Event objects with Type "Alarm History" were not displaying all seven characters in the Alarm worksheet Selection field.
|
960188147 |
1927215 |
Database functions, such as DBExecute(), were not executing successfully when running the functions from Mobile Access for a Windows Embedded installation.
|
960190427 |
1934739 |
EncryptData() and DecryptData() functions were not working in Embedded HMI when called from Background Tasks.
|
960195763 |
1970866 |
Separate Remote Management connections to the Linux runtime were not maintaining consistent hardware identifiers.
|
960200534 |
1997577 |
Alarm/Event objects with Type "Alarm History" were not refreshing on Mobile Access. |
960224137 |
2126520 |
Format function "optStrThousandSep" parameter was not documented correctly. |
N/A |
1708169 |
Applications were not reliably opening if there was an existing VPN connection across network domains. |
These are the issues that were resolved for specific communication drivers.
Case No. |
ID |
Description |
0002179841 |
583606 |
TSAA driver did not support Trident PLCs Firmware v3.1 CIM 3211 Comm Modules, and had slow communication due to smaller read block size.
|
960035991 |
1633552 |
TI500 driver had stability issues and driver logs were incomplete. |
960076816 |
1292850 |
MQTT driver did not support Azure IOT Hub and Amazon Web services IOT Core MQTT brokers. |
960082121 |
1354047 |
DNP driver stopped communicating with fast changing values when using continuous reads for MONITOR events. |
960103571 960215285
|
1471502 2063779 |
COSYS driver did not support Authentication required by controllers that have embedded security management configured.
|
960106829 |
1527207 |
MOTCP driver did not show correct precision for floating point values. |
960107712 |
1502031 |
ABCIP Tag Integration failed when there were structures with unsupported or invalid members. |
960108385 |
1506164 |
OMRON Tag Integration continuously refreshed when verifying the application, creating duplicate classes with different StructureName properties for the imported tags.
|
960109588 |
1503498 |
SNMP driver failed when there were invalid items in a read group. |
960111116 |
1512680 |
MQTT driver when using Sparkplug failed when exceeding 80 tags. |
960117727 |
1591495 |
SCHNE driver was not able to correctly communicate with TOD datatype arrays with overlapping (drift) values. |
960120016 |
1593504 |
CODESYS Tag Integration did not show Enumeration type variables when using Symbol File Browsing (Offline). |
960124628 |
1631832 |
MQTT driver stopped requesting values for fast changing data on the broker and eventually stopped communication.
|
960129901 |
1804357 |
TI500 was not able to consistently reestablish connections. |
960136124 |
1662656 |
ABCIP driver in physical mode was reading and writing to invalid array indexes. |
960140258 |
1687602 |
COSYS and SOMAC drivers were reading incorrect values for Enumeration type tags. |
960140264 |
1687393 |
ABCIP driver did not create groups for string tags correctly. |
960144436 |
1730279 |
MELSE driver on Linux runtime did not communicate when there were two or more PLC stations on the main driver sheet.
|
960146100 |
1725158 |
TWCAT Tag Integration was not correctly parsing tags when there were some invalid tags. |
960146359 |
1710667 |
MELSE driver was not correctly reading from and writing to bits of word registers. |
960148214 |
1733097 |
SIETH and SITIA secure PG/PC and HMI communication option was not documented. |
960148279 |
1717513 |
OMETH driver on Linux runtime was not able to communicate correctly and always returned Status Code "-15". |
960149236 |
1736303 |
In ABCIP physical mode, string tags that expected Date and Time values were reading "0". |
960150498 |
1731502 |
OMETH driver on Linux runtime printed out debug trace messages to the log. |
960150512 |
1731513 |
OMETH driver halted Linux runtime on devices with x86 architecture. |
960155494 |
1775829 |
MQTT driver was not correctly reading Arabic strings. |
960156831 |
1789107 |
SNMP driver was not communicating correctly with secure and authenticated SNMP v3 devices. |
960167935 |
1838041 |
SCHNE driver did not correctly read or write to boolean members of structs with mixed data types. |
960193313 |
1964247 |
IE104 driver did not support multiple Common Addresses on Station for a single driver instance. |
N/A |
584623 |
MOTCP driver could not read or write strings of 82 or more characters. |
N/A |
1996079 |
OMETH driver was not validating source node number on Windows or Linux runtimes. |
N/A |
2036341 2047710
|
MQTT 'Write Status', 'Write Completed', and 'Read Status' were not functioning correctly. |
This is a list of known issues that remain in this version, with appropriate contingencies and workarounds.
ID |
Description |
---|---|
1135583 |
Issue: Only the first 512 characters of a String tag are saved when selecting the Retentive Value string tag property for projects running in the Embedded HMI runtime edition on Windows Embedded. Workaround: Limit String tags to 512 characters when running projects in the Embedded HMI runtime edition on Windows Embedded.
|
1631020 |
Issue: Some communication drivers (e.g., MODBU) have not yet been improved to support long strings, which means they are limited to 81 characters per read operation. Workaround: Divide long strings into shorter strings of 81 or fewer characters per string, and then store those shorter strings in multiple device registers.
|
1788460 |
Issue: Screen viewer performance suffers if SetTagDisplayUnit function is called more than 21 times by a screen. Workaround: Limit the number of times a screen calls to function SetTagDisplayUnit to 21 or fewer.
|
2400387 |
Issue: On Mobile Access, when the zoom mode is disabled, the user is able to do touch gestures on the screen to zoom in, zoom out or navigate over the screen content. On iOS devices, if you do this and your finger touches an object that has a command assigned to it, this command will be executed. |
N/A |
Issue: Text Box objects are drawn incorrectly in project screens that are viewed through Mobile Access. This might be due to scaling of the user interface. As computer displays have achieved higher resolutions, operating systems have implemented UI scaling to ensure that text, apps, and other items are displayed large enough to be usable. However, this UI scaling can affect the behavior of some apps, especially those that include drawing or rendering functions. Workaround:
|
More than one major version (for example version 8.x or 2020) of Ecostruxure Machine SCADA Expert can be installed on the same computer, because each major version is installed in its own appropriately named program folder. For example, this major version is Ecostruxure Machine SCADA Expert 2020, so by default it is installed in the following location on your hard drive: C:\Program Files\Schneider Electric\EcoStruxure Machine SCADA Expert 2020
Many users keep a previous major version installed on their computer while they become familiar with the changes in the latest major version. You can run only one version at a time, however, so you should remove the previous version when you no longer need it. If you are installing a service pack or patch to an existing version, it will update that version, not any other versions you have installed.
When you upgrade from a previous major version to the latest major version, you also need to upgrade your software license(s). To purchase a license upgrade, contact your software distributor. To apply that upgrade to the software, use the Protection Manager utility that is installed with the software (Start > Ecostruxure Machine SCADA Expert 2020 > EcoStruxure Machine SCADA Expert 2020 Register). For more information about licensing, see the Help Manual.
If you do not upgrade your software license(s), it will still run in its full-featured Evaluation Mode for up to 40 hours. After that time expires, however, you can only run the software in its limited Demo Mode.
When you update a major version to its latest minor version, you do not need to update your software license(s). The license is for the major version, so it includes all of the subsequent updates, patches, and hot fixes for that major version.
Finally, when you open an existing project for the first time in a new version, that project is automatically and permanently updated to the new version. This is true regardless of whether you have upgraded your software license(s). Therefore, you should back up your existing projects before you open them in the new version. Each major version of the software creates a corresponding projects folder (e.g., Ecostruxure Machine SCADA Expert 2020 Projects) in your user directory, so you can simply copy (not move) your projects from the old projects folder to the new projects folder.
This section describes the system requirements and additional considerations for installation to develop projects, or to use the computer as a project runtime server and/or thin client.
Standard Requirements
Optional Items
This item is optional because softkey licensing is also available.
This item is optional because many newer device protocols use Ethernet communication (TCP or UDP) instead of serial communication.
One of the following operating systems:
Use the Pro (Professional) or Enterprise editions of Windows because they include Internet Information Services (IIS) as a pre-installed feature that can be turned on. Do not use the Home and Education editions of Windows, because many features are hidden or disabled in these editions.
You can install the full software on a Windows Embedded device, as long as it meets the system requirements listed above. If you do not plan to develop projects on that device then you should install Embedded HMI instead. For more information, see the help manual.
Update Windows before you install the software in order to have the latest security fixes and system components.
You need to have both .NET Framework 3.5 and .NET Framework 4.8 (or later) installed and enabled.
If Windows is fully updated on your computer, the latest versions of .NET Framework should be installed, but they might not be enabled. Use either the Windows Features control panel in Windows or the Server Manager console in Windows Server to confirm that both versions of .NET Framework are enabled.
In some cases, it might not be possible to update Windows through normal means. For example, if your computer is on a private network without access to the Internet, it might not be able to contact the Windows Update service. You can use another computer to download an offline installer for each .NET Framework and then transfer it.
This item is optional because it is not required to develop a basic project and then run it on a standalone device, but it is required to use more advanced features.
This item is optional because you can always use the built-in Viewer program to view project screens.
This item is optional because you can always use the built-in Viewer program to view project screens.
Previous versions of Internet Explorer are no longer supported. In some cases, you can use Microsoft Edge in Internet Explorer (IE) mode, which enables backward compatibility for legacy websites and applications like Web Thin Client. It is supported with limitations, however, and you might see unexpected behavior while viewing project screens. For more information, go to: https://www.microsoft.com/en-us/edge/business/ie-mode
The operating system, storage, and memory requirements will necessarily increase for larger projects; the minimum requirements listed above are only for projects of up to 4,000 tags. The following table shows the complete requirements:
Project Size |
Operating System |
Storage |
Memory |
---|---|---|---|
up to 4,000 tags |
Windows, Windows Server, Windows Embedded Standard
|
2 GB available |
1 GB available |
up to 64,000 tags |
Windows, Windows Server
|
4 GB available |
2 GB available |
up to 10 million tags |
Windows Server only (multi-core)
|
8 GB available |
4 GB available |
Your computer needs to meet only the minimum requirements when you first install the software and begin to develop your project, but the requirements will increase as your project grows. Every computer or device that you plan to use as a runtime station is subject to the same requirements.
If you are using Industrial Graphics screens, the project should be hosted on a dedicated Windows system with IIS installed. The additional system recommendations for this dedicated system are:
These recommended requirements are suitable for a system with ten clients, browsing pages with approximately 40 dashboard/charting components with ~250 I/O tags on the page. Pages may take a longer time to display on the first visit. The display time depends on graphics and script complexity. Additional clients can be supported by increasing the number of CPU’s, CPU speed, and Memory.
You need to have administrator privileges on your computer in order to install any software. If you are not already signed on as a user with administrator privileges when you run the software installer, you can choose to run the installer as an administrator. To do this, right-click the installer program file (setup.exe), and then on the shortcut menu, click Run as administrator. You will be asked for the appropriate user name and password.
On the Select Features page of the installation wizard, you can select which features and software components to install. If you deselect features that you know you will not use, you will decrease the amount of hard drive space required for installation.
Feature |
Description |
---|---|
Program Files |
The main program files for the project development environment, the project runtime software for Windows and Windows Server, and the thin client software for viewing project screens. You cannot deselect this feature.
|
Custom Widget Framework |
Additional software that is required to develop HTML5-based widgets and then use them in project screens. You cannot deselect this feature.
|
AVEVA Historian |
Additional software that is required to save historical data from your project to an external database, such as AVEVA Historian. If you want to use this feature in your project, you must have .NET Framework 4.8 (or later) installed and turned on.
|
BDE for PanelMate™ Import Wizard |
Borland Database Engine (BDE), which is required to import a PanelMate Plus or PanelMate Power Pro program into a new project. This feature is not selected by default, because it is used only in some cases.
|
Demo Projects |
Pre-made projects that demonstrate the product capabilities.
|
Hardkey Support |
Additional software that supports the use of Wibu-type hardkeys (a.k.a. dongles). You may deselect this feature if you are using either Sentinel-type hardkeys or softkey licenses. For more information, see Third-Party Software below.
|
Industrial Graphics |
The Industrial Graphics editor and symbol library, which works as a companion to our native graphics tools.
|
Mobile Access Runtime |
Add-on software for Internet Information Services (IIS) that lets you use HTML5-compatible browsers to view your project screens. If you select this feature, the installer will try to confirm that IIS is installed and turned on in Windows, and if it is, the add-on software will be installed. Regardless of whether you select this feature for installation, a separate Mobile Access Runtime software installer (MobileAccessSetup.exe) will be copied to your program folder. You can run that installer at a later time.
|
OPC Components |
Additional components that are required for communication with other OPC-compatible devices. This includes OPC DA (a.k.a. OPC Classic), OPC XML-DA, and OPC UA.
|
PDF Printing |
Additional software that lets projects save runtime reports as PDF files.
|
Runtimes – Additional > IoT View |
This is the platform-agnostic project runtime software for Linux and other operating systems. Selecting this feature will not actually install IoT View on your computer at this time. It will only copy the installation files to your program folder, so that you can install IoT View on another computer or device at a later time.
|
Runtimes – Additional > Windows Embedded Standard |
Also called Embedded HMI, this is the project runtime software for Windows Embedded Standard computers. Selecting this feature will not actually install Embedded HMI on your computer at this time. It will only copy the installation files to your program folder, so that you can install Embedded HMI on a Windows Embedded Standard computer at a later time.
|
Runtimes – Additional > Windows Embedded Compact |
Also called Compact HMI, this is the project runtime software for Windows Embedded Compact devices. Check the manufacturer's documentation for your device to see which processor it uses. Selecting this feature will not actually install Compact HMI on your computer at this time. It will only copy the installation files to your program folder, so that you can install Compact HMI on a Windows Embedded Compact device at a later time.
|
Symbol Library |
A large library of pre-made but customizable screen objects such as pushbuttons, toggle switches, gauges, dials, and indicator lights.
|
The installer creates a shortcut on your desktop and adds the following items to the Start menu:
Item |
Description |
---|---|
EcoStruxure Machine SCADA Expert 2020 Help Manual
|
A complete technical reference and user guide.
|
EcoStruxure Machine SCADA Expert 2020 Quick Start Guide |
A brief, printable guide to the project development environment, including a step-by-step tutorial for how to develop and deploy a simple project.
|
EcoStruxure Machine SCADA Expert 2020 Register
|
A utility program that you can use to view and change your software license settings.
|
EcoStruxure Machine SCADA Expert 2020 Release Notes
|
The document that you are reading now.
|
EcoStruxure Machine SCADA Expert 2020 Remote Agent
|
A utility program that lets other stations remotely manage the project runtime when it is running.
|
EcoStruxure Machine SCADA Expert 2020 SCADA
|
A shortcut that automatically runs the most recently opened project.
|
EcoStruxure Machine SCADA Expert 2020 Studio |
The project development environment, project runtime and/or project viewer. Its actual capabilities are determined by your software license settings.
|
Third-party software components are installed and added to Windows > Control Panel > Programs > Programs and Features. Do not manually uninstall any of these items until after you have uninstalled our software.
Item(s) |
Description |
---|---|
Microsoft Visual C++ Redistributable (multiple versions) |
These items are required to run C++ applications that were developed using Visual Studio. Several different versions (e.g., 2012, 2013, 2015–2019) may be installed. Do not uninstall these items; they may be used by other applications.
|
novaPDF SDK 10 Printer Driver novaPDF SDK 10 COM (x64) novaPDF SDK 10 COM (x86) Studio PDF3
|
These items let projects save runtime reports as PDF files. They are installed when you select the PDF Printing feature for installation; for more information, see Selectable Features above.
|
Sentinel Protection Installer 7.6.9 |
This item supports the use of Sentinel-type hardkeys (a.k.a. dongles). It is always installed regardless of whether you select the Hardkey Support feature for installation; for more information, see Selectable Features above.
|
CodeMeter Runtime Server
When you select the Hardkey Support feature for installation, Wibu Systems' CodeMeter Development Kit is installed on your computer. It supports the use of Wibu-type hardkeys (a.k.a. dongles). These hardkeys are offered as alternatives to Sentinel-type hardkeys. For more information about the differences between Sentinel and Wibu, ask your software distributor.
Unlike the other items described above, CodeMeter Development Kit is not added to the control panel Programs and Features. It runs as a background process named CodeMeter Runtime Server, which you can find in the Windows Task Manager.
When you uninstall our software, CodeMeter Development Kit is also uninstalled automatically.
This section describes issues that might occur during installation.
"Failed to complete script based install"
You might receive the following message during installation: "Error 1628: Failed to complete script based install." For more information about this issue and how to resolve it, go to: https://community.flexera.com/t5/InstallShield-Knowledge-Base/Error-1628-Failed-To-Complete-Script-Based-Install/ta-p/4014
"CodeMeter Development Kit is already installed"
If you try to install an earlier version on a computer that already has a later version installed, you might receive the following message during installation: "Version x.x.x.x of CodeMeter Development Kit is already installed. Downgrading to Version x.x.x.x is not possible, installation will be aborted." CodeMeter is supplemental software used to manage hardkey licenses. To resolve this issue, use Task Manager in Windows to stop CodeMeter Runtime Server (CodeMeter.exe) before you install the earlier version.
"The local print spooler service is not running"
If you select the PDF Printing feature for installation but the Print Spooler service is not running on your computer, you might receive the following message during installation: "The local print spooler service is not running. Please restart the spooler or restart the machine." You can select OK to acknowledge the message and finish the installation, but the PDF Printing feature will not be installed correctly. To resolve this issue, do the following:
Restore from a System Restore point
If the installation fails for any reason, you can use the System Restore feature in Windows to revert your computer to a previous restore point.
The following documentation is installed in the program folder, which means you do not need an Internet connection to access it:
Document |
Description and Location / Access |
Release Notes (Readme.html) |
This is the document that you are reading now, and it summarizes product news and installation information. These notes are revised for each update (e.g., version 20.0.3), but not for each patch (e.g., version 20.0.3.1). To access this document:
|
Help Manual (TechRef.chm) |
The help manual provides comprehensive and searchable help for the project development environment, instructions for how to develop and deploy projects, and complete descriptions of all of our built-in functions. To access this document:
|
Quick Start Guide (QuickStart.pdf) |
The Quick Start Guide provides a tour of the project development environment, descriptions of essential concepts, and a simple project development tutorial. All of this information is also included in the Help Manual. To access this document:
|
Driver documents (<driver name>.pdf) |
Each communication driver has its own document that describes the protocol used by the driver, how to configure the communication settings for the driver, how to format station IDs and I/O addresses in driver worksheets, and any other technical requirements for connected devices. If you download an updated driver package from our website, that package should include an updated driver document. Each driver has its own separate <driver name>.pdf docment. For example, the driver document for the basic Modbus driver (MODBU) is MODBU.pdf. To access there documents:
|
License document (License.pdf) |
The License document provides legal information regarding your license to use EcoStruxure Machine SCADA Expert 2020. You are asked to agree to this document when you install the software. To access this document:
|
Copyright document (Copyright.pdf) |
The Copyright document provides legal information regarding the copyrights of the incorporated third-party software. You are asked to agree to this document when you install the software. To access this document:
|