RELEASE NOTES for Schneider Electric Device IP Configuration Utility Revised: April 2021 Affected Revision Levels: ----------------------------------------------------------------------- Schneider Electric Device IP Configuration Utility v5.0.4 ----------------------------------------------------------------------- The Device IP Configuration Utility is a Windows application designed specifically to remotely configure the basic TCP/IP settings of Network Management Cards. The Device IP Configuration Utility runs on Windows(R) 2000, Windows 2003, Windows Vista, Windows XP, Windows 7, Windows Server 2008, Windows 8 and Windows 2012. _______________________________________________________________________ Table of Contents: _______________________________________________________________________ 1.0 Schneider Electric Device IP Configuration Utility v5.0.4 1.1 COMPATIBILITY 1.2 KNOWN ISSUES IN THIS VERSION 1.3 NEW FEATURES & ENHANCEMENTS SINCE v5.0.3 1.4 BUGS FIXED IN THIS VERSION SINCE v5.0.3 _______________________________________________________________________ 1.0 Schneider Electric Device IP Configuration Utility v5.0.4 _______________________________________________________________________ 1.1 COMPATIBILITY ----------------------------------------------------------------------- The Device IP Configuration Utility runs on Windows(R) 2000, Windows 2003, Windows Vista, Windows XP, Windows 7, Windows Server 2008, Windows 8 and Windows 2012. 1.2 KNOWN ISSUES IN THIS VERSION ----------------------------------------------------------------------- None. 1.3 NEW FEATURES & ENHANCEMENTS SINCE v5.0.3 ----------------------------------------------------------------------- The packaged Java Runtime Environment (JRE) was removed from the bundle. Instead, we looked at the best practices for Java apps on Windows, and the majority now use an independent JRE configured on the host machine to prevent distributing older software which may have bugs/security issues of their own. In this way, the end user can maintain an up-to-date Java environment without having to wait for a software release from us. The Device IP Configuration Utility has been modified to function in this manner. It checks for an instance of Java 1.8 or higher on the host machine. If Java is not installed, or is older than 1.8, the utility will display the message below (note that this is a standardized message from the java executable windows wrapper.) Clicking “OK” opens the most recent Java download. 1.4 BUGS FIXED IN THIS VERSION SINCE v5.0.3 ----------------------------------------------------------------------- Fixed a bug with newer JREs where a binding error could be displayed even in the case of a successful IP assignment.