Brief Guide to ICD File Name Conventions and Patterns
=====================================================

E1 stands for Edition 1 of the IEC61850 standard.
E2 stands for Edition 2 of the IEC61850 standard.

From the "IEC 61850 and ION Technology" publication:
---------------------------------------------------------------------
The ICD file is a template that defines the IED (such as your meter) in terms of its capabilities. Be sure to select the ICD file that matches your meter type and hardware configuration.

	Example ICD file name: SE_PM8000-Onb1-Exp1-Exp2-Exp2-Exp2-F01_E2V01.icd

EXP1 corresponds to the Digital option module METSEPM89M2600.
EXP2 corresponds to the Analog option module METSEPM89M0024.

Option card configurations are listed from slot A (closest to the meter), to slot D (furthest from the meter).