V3.40 SMALL : TLXCDSUOFS34 TLXCDSTOFS34 OFSCSPESU OFSCSPEST OFSCSPBSUSSC OFSCSPBSTSSC

V3.40 LARGE : TLXCDLUOFS34 TLXCDLTOFS34 TLXCDLFOFS34 OFSCSPELU OFSCSPELT OFSCSPELF OFSCSPBLUSSC OFSCSPBLTSSC OFSCSPBLFSSC

OPC Factory Server V3.40

IE2812 SP4

Copyright © 2003-2013 Schneider Electric Industries SAS


Enhancements - Bug Fixing :

2809 Server SP1

Enhancement : Retry mechanism on datadic loading has been enforced to ensure loading completion on communication failure.

2810 Server SP2

Bug fixing : when Quick Item Validation was checked, a missing device used to be abusively reached on AddItems or ValidateItems operation.

2811 Server SP3

Enhancement :  XML parser cyber-security vulnerability fix. OFS XML documents could be compromised by malicious insertion of external references (external information not contained in the original document).This enhancement disables any external references parsing.

2811 Configuration tool SP3

Enhancement :   XML parser cyber-security vulnerability fix.

2811 Shared components SP3

Enhancement :   XML parser cyber-security vulnerability fix.

2811 OPCUA wrapper SP3

Enhancement :   XML parser cyber-security vulnerability fix.

2812 Server SP4

Enhancement : Modicon M580 family support

Bug fixing : When single item activation option is set, removing items used to be badly managed.  

Bug fixing :  Data type checking enforcement on Data dictionnary reloading

 


 

The actual OFS 3.40 Server and Configuration tool should be installed. (optionally OPC-UA wrapper)

If OFS3.40 LARGE is installed, the LARGE\Server folder content must be copied in the x:\Program Files\Schneider Electric\OFS\Server folder .

If OFS3.40 SMALL is installed,, the SMALL\Server folder content must be copied in the x:\Program Files\Schneider Electric\OFS\Server folder

The OFSConf folder content must be copied in the x:\Program Files\Schneider Electric\OFS\OFSConf folder It is strongly recommended to archive the current OFS Configuration before that operation.

If UNITY PRO is not installed or if UNITY PRO with version < 6.0 is installed, the SRCSDK51 folder content must be copied in C:\Program Files\Common Files\Schneider Electric Shared\SRCSDK folder.

If UNITY PRO with version >= 6.0 is installed, the SRCSDK60 folder content must be copied in the C:\Program Files\Common Files\Schneider Electric Shared\SRCSDK folder.

If OPC-UA wrapper is installed, OPCUA folder content must be copied in the x:\Program Files\Schneider Electric\OFS\OPCUA folder.

All other components of OFS v3.40 remain identical and are thus not delivered.